Part Number: EVM430-F6779 Hi experts,
My customer would like to perform 3-phase 4-wire measurements using EVM430_F6779 and EMDC .
We think EVM430_F6779 supports the Neutral terminal as a hardware, but the EMDC(1_40_00_03) sample software does not. Could…
Part Number: EVM430-F6779 Other Parts Discussed in Thread: MSP-FET , I am working with the MSP430(EVM430-F6779) evaluation module. do i compulsory need the debugger(MSP-FET) to program the EVM.
Does only launch pad along with isolater is enough to program…
Part Number: EVM430-F6779 Other Parts Discussed in Thread: MSP-FET , MSP430F5529 Hi
Does the EVM comes preprogrammed.?
How to program the EVM?
Can we use TI launch pad for programming the EVM. If so please detail the steps involved.
Hi Luke,
Thank you for the reply. Sorry for the additional question.
Luke Ledbetter said: Though not calculated like this in the library, the power factor should also be equal to the cosine of the phase angle.
Q1:What exactly is a library? (Energy Measurement…
Hi Eason,
Sorry for late reply.
Thank you for the information. I am still in the process of confirming the information I received, but please let me ask question.
Eason Zhou said: Q4:Does EVM perform calculations assuming a Y connection or a Δ connection…
Part Number: EVM430-F6779 Hello TI team,
I am using evm430f6779 energymeter. I want to see the current and voltage measured values in the serial monitor of PC using UART. How can i do that ? where i can make changes in the energymeter code ?
From source…
Part Number: EVM430-F6779
Hello TI team,
at my company we are making other type of energymeter by using the TI's energymeter. But we have only few changes in the hardware. Because of that i have to make changes in the code.
If we are using the different…
Part Number: EVM430-F6779
Hi,
I am working on the EVM430-F6779 after flashing the default code ( EVM430-F6779_CT_3V_3C_50Hz.txt ) into the EVM, the LCD functionality is not working. The other parameters like V, I, PF, KWH etc are displayed in EMDC GUI…
Part Number: EVM430-F6779 Other Parts Discussed in Thread: MSP-EXP430F5529LP , MSP-ISO , MSP-FET I Connected Source and load to the EVM430-F6779 but not able to see the display ON(Device Didn't Boot up). Could you help us how to power up this device and…
Part Number: EVM430-F6779
Hello,
I connected the EVM to PC through RS-232 connection. using the steps mentioned in the below documentation.
https://www.ti.com/lit/an/slaa577g/slaa577g.pdf
i can only see the button is red.
I verified the connections even…