Part Number: ADS1299 Tool/software: I bought a EEG signal generator that can generate low-frequency small signals, and I want to verify the correctness of my acquisition board. The signal generator is set to output a sine signal with an amplitude of 50UV…
Part Number: AM3351 Tool/software: We’re observing spurious data in the receive buffer for UART1 on the AM3351 (ttyS1 under Linux) configured as RS485, using the Linux SDK 9 kernel and toolchain (ti-processor-sdk-linux-am335x-evm-09.01.00.001, arm-none…
Thank you for your response.
Below is the datasheet of the SiC MOSFET.
In this case, could you advise what VDD voltage would be appropriate if I supply VDD power through the auxiliary winding?
Also, I’m still not fully confident that I understand…
Part Number: AMC1400-Q1 Other Parts Discussed in Thread: AMC1400 , AMC1411 , AMC131M01 Tool/software: I'm currently designing a high-side current sensing stage for a system with a working voltage of up to 4300 V , and I need to ensure at least 5300 V…
Hi Santosh,
Thanks for your reply. I too thought that this would give the desired output, however I found it to actually be slightly different. As shown below, when I set the periodicity of subframe 0 to 50 ms and of subframe 1 to 200ms, it outputs…
Hi Naoki-san,
Yes, reflections will occur at the input to PkgIN.s4p but the degree is important to note. If one clicks Check/View S-Parameters and notes S11 and S22 at low frequencies like 250 MHz, the return loss is not measured. The return loss at…
Part Number: DRV8706-Q1 Tool/software: Hi Sir, My customer is using the DEV8706S-Q1 to drive a TCM motor module, they found when the operate frequency over 12kHz, the high-low side gates both have the short phenomenon. They measured the abnormal waveform…
Part Number: TPS4800-Q1 Hi Team,
Use TPS4800,
There is currently a MOS drive issue with a voltage of 33V, 1. R11:10K, R13:0R, R14:10R, C4:15nF, C3:1uF, When there is no external load capacitor, using the battery to power on the TPS4800 switch is normal…