Part Number: IVC102 We have performed 20 ABA test. When we take an old IVC102 from 2018/2020 and swap with an IVC102 from 2021/2023 the problem follows the IVC102.
Something has changed. The 10pF option has a much larger variation in measurement values…
The RS-232 specification requires a driver to output at least ±5 V when connected to a load of 5 kΩ ± 2 kΩ. The MAX232E conforms to this specification.
The MAX232E deliberately limits the output current to limit the slew rate to 30 V/µs, and is guaranteed…
Part Number: BQ76942 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Hi
I have a problem in balancing cells pin, I used 9 cells and I customed BQ 76942 by tied VC10 to VC9. I set up in BQ76942_Init() followed by some codes below:
BQ769x2_SetRegister…
Part Number: BQ27742-G1 Tool/software: output voltage of battery pack drop to 2V and resets quickly back to 4V. This only happens when the battery is installed in the device and I2C is connected but does not occur when battery is externally tested and…
Part Number: AWR2243 Other Parts Discussed in Thread: MMWCAS-RF-EVM Hello TI Team,
I am using a cascaded radar setup MMWCAS-RF-EVM with 4 AWR2243 devices and a TDA capture card on MMWCAS-DSP-EVM . I am working with given Lua scripts for configuring…
Part Number: BQ27Z746 Other Parts Discussed in Thread: EV2400 Tool/software: I am reposting this here as I posted this detail under wrong part number...
our customer is seeing our battery output voltage drop to 2V momentartly (roughly for 1 sec) and…
Part Number: TLC556 Other Parts Discussed in Thread: NA555 , , TPL5110 , LM339 , TLV4082 , TPL5111
Tool/software:
Desired function waveform.pdf NA555, NE555, SA555, SE555 Precision Timers (Rev. I).pdf
Hello
I forgot to include some information…
Part Number: SK-TDA4VM Tool/software: Hello,
I am trying to test max throughput of the TDA4 using mobilenet_v2 and resnet18 models.
I can easily convert onnx file to tidl artefacts with batch size 1 and more. But when I try to run the model. It through…
Fullscreen
8863.test.log
Download
Mon Oct 13 15:30:45 CEST 2025
Device Version Info = 1746_0_01
BQZ Device Name = bq27z746
BQZ Firmware Version = 0_01
Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current…