Hi Suren ,
Please find the register dump of codec for page 0 and page 1
in working case with 16khz
root@myd-am62x:~# i2cset -f -y 1 0x18 0x00 0x00 root@myd-am62x:~# i2cdump -f -y 1 0x18 No size specified (using byte-data access) 0 1 2 3 4 5 6 7…
Part Number: MSPM0L1106 Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi Team,
Our product PCB with MSPM0L1106 was ready recently. I tried to program the firmware to MSPM0L1106 through the onchip BSL by using UniFlash, v9.0.0.5086.
The…
Part Number: SFRA
Tool/software:
The official manual "SPRUIK4A-User's Guide" was ported, and the content of Running Software Test Bench Example for SFRA in the article was also referenced.
First I checked the STB routine of the original demoF28049…
Hi Zeynep,
I believe this is coming from a timing issue related to the sector erase in your flash kernel. I have attached a version that uses bank erase to erase all of flash before downloading and programming the data, can you try this?
Best,
Alex…
Hi, Jared,
Please check update below
Test #01: Postpone ECC_CK enable to A72 u-boot prompt
Seems that it's ok to enable ECC_CK at runtime, but ECC error interrupt is not triggered normally.
// 01. R5 u-boot config ECC protected area 0xD000…
Part Number: LP-EM-CC2340R5
Tool/software:
I am currently using the Host Test Example Code , and the environment and parameters are configured as follows. The code compiles successfully.
When I execute the SCAN command using B Tool v1.44.04 , I…
Part Number: LP-MSPM0L1306 Other Parts Discussed in Thread: UNIFLASH , MSPM0L1306 , SYSCONFIG Tool/software: Hello, I'm using UniFlash to program the MSPM0L1306 using serial programming.
At some point I generated a TI-TXT file which failed loading.…
Hi Josh, recently I was checking out the data at baud rate 500000 by updating the presence_detect profile and I had flashed the evm with presence_motion_detection image. I have saved the data coming at uart terminal, after sending the config a series…
Hello Chagai,
Looks like the microcontroller aboard the EVM may not be programmed with any firmware or may have been wiped at some point. Anyways, I appreciate you showing the drivers helps a lot, so good news the computer recognizes the microcontroller…