Part Number: MMWCAS-RF-EVM Tool/software:
Regarding the MMWCAS-RF-EVM, we were informed via E2E that it does not comply with European standards.
MMWCAS-RF-EVM: Telecommunications Standards - Sensors forum - Sensors - TI E2E support forums
Does it comply…
Part Number: CC1310 Tool/software:
I have been working on the current RF CC1310 project implementing asynchronous transmission and reception, while I am thinking about some problems in my development, I am wondering how to differentiate between asynchronous…
Part Number: AM4376 Tool/software: We are looking a microcontroller which we can be use for one of our development activity which includes the following Interfaces.
We need a MCU with following Inbuilt One-stop solutions with a proven LoRaWAN® stack…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK
I'd like to communicate between TWO cc2530s after getting the value of ADC?
so I need the example of adc and rf communication.
I can't find in the zstack 3.0.
i followed the exact steps of the cascade user guide. It obviously is written for a earlier version, as SW and FW versions are outdated and I got instructed to install newer versions of MMwaveStudio and DFP. Is there a updated version of the cascade user…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243 Tool/software: For the MMWCAS-RF-EVM that we purchased before, we are considering acquiring a special system to use it in experiments. exp-sp.denpa.soumu.go.jp/.../
In order to receive…
Part Number: CC2652P7 Tool/software: Hi,
Customer is doing stability test, fast temp change between -40~85.
Zigbee protocol. ZR role.
if 30s network sync, the device's RF has issue to communicate. looks the PLL is unlocked based on the snapshot of Spectrum…
Part Number: CC2640R2F Tool/software: hello
Is there a way to adjust the interval in the Smart RF Studio Continuous TX section?
Or, I wonder if it is possible to activate unmodulate in the packet TX part.
Currently, we need to measure the BLE communication…
Part Number: LP-CC2652RB Tool/software: Can the "Socket" communications in the Smart RF Sniffer be used to send BLE sniffer data to a device with generic TCP socket communications? For example: an industrial PLC with Ethernet. If so, does the device…
Part Number: CC1200 Tool/software: We are using CC1200 module, configured at 916MHz. As part of our testing, the PCBs with proper enclosure go through a thermal cycling test to verify any board level issue:
1. -35 to +55 degree Celsius with (3-degree…