Part Number: TMS320F28379D Tool/software: Dear Ti Team,
I am using TMS320F28379D development board for R&D activities
would like to seek your support for Digital controller for EV charger Product development,suggest/help me to select TI DSP processor…
Part Number: TPL0401B-10 Other Parts Discussed in Thread: BUF802 Tool/software: Hi, I have a project with BUF802 where I need to use a digital potentiometer with I2C and 1 channel to select the bias current resistor.
The problem is that uC and Digital…
Part Number: DAC8742H Tool/software: I am currently using a DAC8742H as a HART modem and was wondering about the behavior of the digital reset input. I plan to use the DAC8742H in UART mode and never change the configuration inputs (XEN, CLK_CFG0, IF_SEL…
Other Parts Discussed in Thread: UCD9090 I've been using the Fusion Digital Power Designer to program UCD9090. Now I want to automate this process by exporting the firmware upgrade script. However, when I tried to export the script, there was always the…
Hi Brandon,
Thanks for confirming. MCU/MPU will be on separate power supply, I will use isolators in between PSE and MCU/MPU. Also to down convert from 48V to 3.3V, I plan to use LMR36500 which as output current of upto 50mA, is this fine or an LDO is…
Part Number: UCD90120A Other Parts Discussed in Thread: UCD90120 I am attempting to modify an existing Fusion Digital Power Designer project (device is the UCD90120). The device is not connected, so I'm in offline mode. Everything seems to work fine…
Part Number: MSP432E401Y Tool/software: Please have a look at Fig. 17 in U.S. Patent 10,380,986; Fig. 16 in 10,810,986; Figs. 10, 11 & 21 in 11,087,731; Fig. 53 in 12,020,674; and Figs. 18, 26, 30 & 31 in US2023/0013236 A1. I've been designing…
Part Number: MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3107
Hi Champ,
I am asking if M0 could do digital power segment applications, such as power stage controller ?
Besides having corresponding peripherals need for sensing, timer as epwm and…