Part Number: HD3SS2522 Other Parts Discussed in Thread: HD3SS3220 Can this device be used to convert a USB 3.1 Gen 2 port on a host processor to USB Type C? Are full Gen 2 speeds (up to 1212 MB/s) supported not just Gen 1?
thank you
SBU pins are not used by the HD3SS2522. You can connect SBU pins of Type-C receptacle to 1M-ohm pull-downs. You can connect RST pin to a pull-up .
Regards,
Brian
Part Number: HD3SS2522 Hi Sir
I am confused for HD3SS2522 schematic, EVM board with datasheet I / O signal trace is somewhat different. Please refer to below. 1. As shown in datasheet suggested schematic signal trace, pin 2 & 3 and 5 & 6 with pin 44 & 43…
Part Number: HD3SS2522 Other Parts Discussed in Thread: TPS2046B Team,
I checked the CC1/CC2 voltage rating is up to Vcc(3.3V).
But the reference circuit uses TPS2046B to coonect a 5V rail to CC1 and CC2 while VCTRL1/VCTRL2 is low.
Is the setting correct…
Other Parts Discussed in Thread: HD3SS2522 , HD3SS3220 Hi Team, I would like to ask about HD3SS3220 and HD3SS2522. - HD3SS3220: DRP controller with 10G SS MUX - HD3SS2522: DFP controller with 10G SS MUX I beleieve HD3SS3220 (DRP controller) could be DFP, and …
Other Parts Discussed in Thread: HD3SS2522 Hi Team
I have use HD3SS2522 EVM to test function. but I have some issue on this EVM , Please check my Attachment file.
Colud you help to fixed this issue? HD3SS2522 EVM issue.docx
Other Parts Discussed in Thread: HD3SS2522 Hi Sir
I have two question on for and Vconn on HD3SS2522.
1 : HD3SS2522 have mode pin to setting current , Why HD3SS2522 EVM need put pull high resistance on CC pin ? ( ex : R15 - R20 )
2 : If CC pin change to Vconn…
Hi Team, It seems the schematic of Figure 4 seems that P/N connection of the USB3.1 differential pairs partially swapped. Is it correct? Best Regards, Yaita
Other Parts Discussed in Thread: HD3SS2522 , TUSB321 , TUSB320 , HD3SS3212 Dear Specialists
My customer is considering HD3SS2522 for device side.
According to the datashet, it is described for host side.
Can it be used for device side?
If possible, is there…