Other Parts Discussed in Thread: HD3SS2522 , TUSB321 , HD3SS3212 Please let me know about two point below.
①HD3SS2522 and HD3SS2312 + TUSB321
Are following ciecuit necessary to connect EC (ARM controller IC)?
※Are there necessary to connect A0P/A0N/A1P…
Hi Alexander ,
TUSB542 sill do the flip the pins to accournt for the flip of the cable. However you need a Type-C detection device to make a Type-C connect and determine the orientation of the cable. The Type-C controller would then drive the control…
Hello Yaita-san,
It is possible to replace the HD3SS2522 using the TUSB321AI + HD3SS3212. Actually, it is a better solution since the TUSB321A is a newer device.
Regards,
Diego.
Part Number: HD3SS3220 Other Parts Discussed in Thread: TUSB8044 Hi team,
I am developing a USB Type C HUB. So, type C will be on the host (PC) and the hub will have type A connector as extension. I'm planning to use HD3SS2522 2:1 USB mux for type C…
Hi Srinivas,
Type-C is only a connector which is capable for USB3.0, USB2.0, DisplayPort, HDMI, Power Delivery, etc, finding a Type-C port on a device doesn't mean this is necessary USB3.0, it could be USB2.0 only, and the solution needed will depend…
Other Parts Discussed in Thread: TUSB8041 , HD3SS2522 , HD3SS3220 , TUSB321 , HD3SS3212 , TUSB322 Hi,
I'm creating a USB Type C HUB. Type C will be on the host (PC) and the hub will have type A connector as extension. I'm planning to use HD3SS2522 2…
Other Parts Discussed in Thread: HD3SS2522 Hello Team,
Please allow me to make sure the pin connection for HD3SS2522 EVM schematic. Below is the schematic in the user's guide. Looking at the high speed signal pins, A0P/A0N and A1P/A1N pins, they seems…
Other Parts Discussed in Thread: HD3SS2522 , TUSB320 , TPS25810 , HD3SS3220 , TPS25740 , TPS25741 Hi, I want to know more USB charger IC type, Could you give some reference ? (For Type C 5V , 3A and no use I2C control) Thank you~~~