Part Number: HD3SS3415 Hello,
According to Revision History section, temperature changed from: industrial temperature range of –40°C to 85°C to: industrial temperature range of 0°C to 70°C.
Is this change only related to performances…
Part Number: HD3SS3415
Hi team, Could you please confirm why HD3SS3415 cannot support USB2.0 application? i saw the post here and it mentioned "USB2.0 signals can be above the maximum operating conditions of this device." e2e.ti.com/.../39755…
Part Number: HD3SS3412 Other Parts Discussed in Thread: HD3SS3415 , Hi Team,
HD3SS3412 & HD3SS3415 These two differences?
I found these two can't see the difference, who can tell me their difference?
thanks
Kevin
Part Number: HD3SS3415 Hello team,
Could you please advise if TI has the following solution.
My customer is looking for a PCIe switch, GEN3. (Max. bit rate, 8Gbps)
The host (SOM) is connected via 16 lanes to 2 FPGA’s are connected, each via 8 lanes bus…
Part Number: HD3SS3415 Other Parts Discussed in Thread: HD3SS3411 Hi My customer is asking if have reference schematic for hd3ss3415? Thank you
http://www.ti.com/lit/ds/symlink/hd3ss3415.pdf
Part Number: HD3SS3415 Other Parts Discussed in Thread: DS80PCI810 The GPU Server Which Support Intel Purley 2S Platform , and Combine 2 PLX8796 PCIE Switches. Implementing CPU0/CPU1 PCIE root switching through TI HD3SS3415 , Which Tuopu as blow:
1.With…
Part Number: HD3SS3415 Other Parts Discussed in Thread: DS90CF366 , , DS90C365A , TS3V713EL Dear Sir,
My customer looking for a 8-bit 2-to-1 mux and HD3SS3415RUAT is in system. It is designed for LVDS different signaling. I was wondering if it can also be…
Part Number: HD3SS3415 Hi, I am planning to use a point to point LVDS interface for source synchronous data transfer over SMA cables between 2 units comprising of FPGA units. The total no. of channels required for this application is around 16 so, I am…
Part Number: HD3SS3415 Hi,
We are having requirement to expend 6 group of (PCIex1 (GEN3)) to 28 group which include 16* GIGALAN, 10* PCIex1 and 2 PCI interface.
Can you help to recommend proper product?
There are some questions:
1. if using GEN2, what…
Part Number: HD3SS3415 Hello Team,
You know our part HD3SS3415 has some NC pins, such as pin 21, 25, 31, 35, 39. Can you connect these pins to VDD or GND? Because of some reasons, my customer connect these pins to VDD or GND. Please help to check it,…