Hello Rohit,
We no longer offer the ADS1230REF boards. As an alternative, you can use either the ADS1232REF (24b version with 2 input channels and multiple gain options) or the ADS1231REF (24b, single gain of 128, includes low side bridge switch).
We…
Hello Daveon,
Thank you so much for the reply!
I want to first correct a statement I made in my original post. I should not have said 4 PDM mic streams. While we do have 4 PDM mics connected, that are only occupying 2 Serial Audio interfaces on the ADC…
Hi Daria Kiseleva,
Typically a bridge is measured ratiometrically, where the excitation source for the bridge is the same used for the reference voltage. Then, any variation in the excitation voltage is seen equally in the input signal and the reference…
Other Parts Discussed in Thread: HSMC-ADC-BRIDGE , ADS4249 , ADS4249EVM Hi,
I'd like to ask for information about "HSMC-ADC-BRIDGE REV C".
Concretely, I need one about pins information.
Although I confirmed the schematic file about the product…
Part Number: INA333 Tool/software: Hi! I am working with INA333 to amplify a wheatstone bridge output voltage. Here is the circuit in KiCAD:
I am testing the circuit with the INA output connected to a stm32f405-microcontroller ADC pin. The output is…
Hi Bjorn,
It may be helpful to take a look at our Temperature-sensor (RTD, thermocouple, thermistor) firmware for precision ADCs:
ADC-TEMP-SENSOR-FW Application software & framework | TI.com
This temperature-sensor linearization firmware provides a…
Patrick,
I will look into this for you. Did you order the HSMC-ADC-BRIDGE card? When you mention "Does not work" can you tell me what the issue was?
Regards,
Jim
Hi Jim,
Thanks for the files.
We are planning to make a HSMC ADC Bridge board to support all 16 bit connection from ADC EVM to HSMC connector. Thus we need to have the board layout file to modify the design. The shared folder only contains the Gerber files…
Hello,
I got the above adapter board here, probably came with one of the AFE's I have recently ordered.
On the website I can download schematics only from REV B only.
Can someone please point me to the schematic REV C? Or is it the same as REV B…
Part Number: TSW1400EVM We bought TSW 1400 with ADC3422EVM board and works normally,
and we would like to know how to direct the LVDS signal from ADC to DAC connector(J4)?
TSW140x user manual:
http://www.ti.com/lit/ug/slwu079d/slwu079d.pdf#page=3
Is…