Other Parts Discussed in Thread: ISO7240CF-Q1 , ISO7241C-Q1 , ISO7240C , ISO7240CF Hi Expert,
According to datasheet of ISO7240CF-Q1/ISO7240C-Q1, ESD protection is defined 4kV (I believe that this spec is Vpeak.).
However, there is no description…
Other Parts Discussed in Thread: ISO7240CF There is a description of “twake” in ISO7240CF datasheet p5.
Please tell me a min and max of “twake”.
Please answer it by December 4.
I would like to know what the ground current/quiescent current is for this device. The datasheet only specifies the ICCx (EN=HIGH) or Ioff (which is only the output current when EN=0V) and this does not give the ground/quiescent current of the device…
You are correct, Calum, the '245 does not provide the classic definition of isolation. For digital isolation, you would have to use one of the ISO7xxx devices, depending on the configuration required. For example, for a 2TX/2RX configuration, the ISO7242C…
Part Number: ISO7240C Tool/software: Hi,
The following items have been changed from revision T (SLLS868T) to revision U (SLLS868U).
• Updated reference from capacitive isolation to isolation barrier throughout the document. →The description "Isolation…
Hi Ning, Thanks for your assistance.
Regarding the 200nS delay. From IC signal to gate we have the 12V to 5V resistive divider, then the ISO7240CF isolator, then the UCC27714 gate driver. Measure delay through the resistive divider and ISO7240:
Around…
Part Number: ISO7240M Other Parts Discussed in Thread: ISO7740 , , ISO7240CF
Tool/software:
Dear Technical Support Team,
Unexpected momentarily glitch(about 2.5V , 8us) on the output during power up, at a time when Vcc2 is at about 2.5V.
See attached…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…
Hi Hyejeong,
These devices have already completed certification. The datasheet update is in progress, but I do not have a firm date to provide. Please see attached certifications for these devices.
E181974-Vol4-Sec6-20260312_CoC.pdf E181974-Vol4-Sec1…