Hi Rebecca,
Thanks for reaching out.
MIPI interface is primarily a differential interface hence, ISO6720 cannot be used for MIPI interface directly. We currently do not have isolators that can isolate MIPI interface without needing additional devices…
Part Number: DS90UB913Q-Q1 Other Parts Discussed in Thread: ISO7821LLS Does TI have any SerDes chips which will comply with EN60601 medical standards?
I'd like to know if there are any SerDes chips that are medical grade? or example, is the DS90UB913 medical…
Hi Aaron,
Sorry for the delay in responding. I was checking with the isolation products team (probably should've reassigned this thread to them!).
There is a solution to achieve isolation for half duplex LVDS. It requires more than one device though…
Hi Shaobo,
Thank you for showing interest in ISO7821.
To make sure we are referring to the same device, could you please confirm if you meant to refer to ISO7821 (digital isolator) or ISO7821LLS (LVDS isolator)? Please note that these devices are very…
Part Number: ISO7741 Other Parts Discussed in Thread: ISO7641FM , ISO7241M , ISO7821LLS Is there any device able to compete with MAX14131? customer need speed up to 150Mbps for VFD application. thanks.
Hi Anand,
Thank you for your reply.
Comparing ISO1176T with ISO7821LL, I found the following differences from their data sheets.
1. ISO1176T is galvanic isolation while ISO7821LL has capacitor isolation. In term of noise rejection, ISO1176T is better…
Quickly find solutions to common questions about isolated interface devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Isolated …