Part Number: LDC0851 Other Parts Discussed in Thread: LDC1101 , TMAG5170 Hi,
I want to use LDC0851 for event counting for paddle wheel systems.The paddle wheel have 5 teeth and rotating about 7000 rpm.
I use pvdf teeth with 316 stainless steel about 1mm…
Part Number: LDC1101EVM Hello, just received the LDC1101EVM board and installed the GUI. The board is listed in Device Manager as "EVM (COM8)", but in the GUI the COM Port pulldown is blank so the evm does not connect. I am using a Windows 10 PC.…
Part Number: LDC1101 VDD is powered from 3.3V digital and ground and the Rp values are excessively noisy. Don't have the common mode filter laid out on the board, so I only have the two 0402 EMI caps on the INA/INB pins to ground to mitigate EMI susceptibility…
Part Number: LDC1101 Hello,
Hope you are well.
I've been using the LDC1000 for position sensing. Recently, I tested the LDC1101. I just wanted a quick confirmation on something.
On the LDC1000, when my sensor is closest to the target (lowest Rp),…
Part Number: LDC1101 Hello everyone,
I am using LDC1101 EVM and am pleased to use it.
It is very accurate and has high resolution.
But I am now decoding the data and cannot understand how to do it.
Below is where I am facing the issue. These are Rp+L…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 , LDC1312
Hello everyone,
I recently bought LDC1101EVM for inductance sensing and want to actually use inductance data coming out from the USB port.
My next problem is how can I communicate…
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: TXU0304 , TXU0104 , SN74LVC1G34 I got some SN74AVCH4T245DR IC samples recently I wanted to use them for shifting level between 5V SPI and 1.8V SPI interface It took a long time to select this IC…
Part Number: LDC1101 Hi All,
I have a question about LDC1101 Please tell me the output impedance values of INA and INB connected to the LC circuit.
Best Regards, Ishiwata
Part Number: LDC1101 Now using LDC1101 for the ranging of metal objects, inductors are using ferrite winding inductors. L:70uH, C:1000pF, Rp 56K s without target. Now there are three issues during debugging 1. Close range (<8mm) measurement is normal, Rp…
Part Number: LDC1101 Hello,
Is it possible to form the resonant LC section with capacitive probe and a fixed inductor or some coax . The resonant frequency would be modulated with the change in capacitance rather than inductance, the LDC1101 wouldn't know…