Other Parts Discussed in Thread: SYSCONFIG , AM3359 Hi,
I am trying to implement the TSC_ADC peripheral of the AM335x in general-purpose mode to digitize 8 different AIs (AIN0 - AIN7). As a foundation for my code, I am using adcVoltMeasure.c, found…
We are using 64-bit F 17 with the latest updates available as of the timestamp on this post.
We followed the instructions that you recommended in your link for installing on the latest versions of Fedora:
Fedora 16 64bit
Download the install file…
Part Number: VFC32 Other Parts Discussed in Thread: TLV3501 Hi,
Does TI voltage to duty cycle modulator as LTC6992MPS6-1#TRMPBF ?
I only can find VFC32, but it voltage to frequency not duty.
LTC6992_1_6992_2_6992_3_6992_4-1270033.pdf
Thanks! …
Other Parts Discussed in Thread: EK-LM3S811 (post is contained in attachment for printable format)
The XDS100 emulator is a low-cost JTAG emulator hardware interface option for interfacing to Stellaris devices when using the Code Composer Studio IDE…
Hi Chris,
The result should be the same between Webench and spreadsheet if that parameter is the same. But the result of total inductance is different.
For example, the result with 1.5mm PCB thickness is 8.76uH in spreadsheet (see attached), but Space…
Hi Cynthia,
Here is the manual of the FPGA dev board (DE10-Lite) for reference. As you mentioned, there are no resistors between the FPGA and GPIO port on the FPGA board (see sheet 31 of the enclosed pdf file DE10-Lite_User_Manual). But there are resistors…
I am sensing 230 voltage with using the LV25-P sensor for ADC of F28335 board. I studied different papers, Like the one attached linked herewith, in which the multiply with 26. I am confused how?. Can somebody share the correct way of scaling/calibration…
Si8410_20_21_Rev_1.5.pdf Sorry for typo. See below,
Hi! Ben,
I am in process of design. And I found in LM5045 application note, (page 25), Ti is using Si8420BB-D-IS, as a digital isolator. But the IC, SI8420 data sheet has a water silk mark "Not Recommended…
Sadly the fix doesn't seem to be that easy - the jumpers were in place. I'm fairly sure the USB port works in general, since it functions as a UART in other examples that I use. The main difference is that the board gets power from the USB when connected…