Part Number: LM111QML-SP Hello,
Would the LM111QML-SP work with a 28VDC supply voltage? The datasheet says 5VDC to +/-15V , but it also says it should be able to switch up to 50V and the positive supply voltage is up to +30V.
Thanks
Part Number: LM111QML-SP Hi experts!
My customer is looking for bench data from a few sample units showing overdrive response with 5mV overdrive.
They are also not sure how the tRLHC and tRHLC parameters are defined. What are the starting/ending points…
Other Parts Discussed in Thread: LM111QML-SP Hello,
Can someone please tell me; on the LM111QML-SP TO-99 is the case of the part connected internally to any of the pins, or is it grounded at all if the lid is metallic etc.?
Thank You!
Hi Harry,
It is confusing. That is due to 40 years of changing standards...
To make it more fun, there are *two* versions of the LM111. The ex-National Semiconductor devices (LM111-N and the QMLV devices) and the "second source" TI devices.
Most…
Hello Furkan,
Here again is the list of dummy packages for space grade products in ceramic packages.
Note that this list is a couple of years old and does not list all dummy packages available. However, newer products will also list the dummy packages…
Hi Furkan,
Below is the table of orderable dummy packages.
Note that this info will be in the next Space Selection Guide to be released soon on ti.com.
The package numbers are also slowly being added to the product pages on ti.com.
Space…
Hello Uriel, The TL331 is the single version of the LM139 family. Unfortunately, it is not available in Space grade. The dual version, the LM193QML-SP is available. If you need a single, the closest single would be the LM111QML-SP.
Hi Tilman,
Welcome to E2E Design Support Community!
We are actually working on updating our TI Space Products Guide (ti.com/spaceguide) to include a list of Dummy Packages / Mechanical Samples, which should be updated in the coming months. In the…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf