Part Number: LM21215 Other Parts Discussed in Thread: TPSM8287B30 We have a design for a MPSOC using the LM21215MH/NOPB to supply the core 0.85V rail which is out for fab. The logic design for the MPSOC PL has grown significantly since the HW was designed…
Part Number: LM21215 Other Parts Discussed in Thread: TPSM8287B30 , Hello team,
My customer would like to change the current limit setting on the field.
Would it be possible to use DAC to set the current limit instead of resistor? Or should we use…
Part Number: LM21215 Other Parts Discussed in Thread: TPS6287B15 , TPS62873 Dear Technical Support, Good day!
Is there a junction to case thermal resistance parameter for LM21215MHE/NOPB ? Please help verify.
Mouser Part #:
926-LM21215MHE…
Part Number: LM21215 HI,
How to read the Gain Margin and Phase Margin from the Bode Plot graph after running simulation with the design?
Thanks,
Laurie
Part Number: LM21215 Hi Team,
As we know, generally speaking, the premise of a stable system is that about 45° phase margin and 10dB gain margin. I noticed about some system is still stable even if when -180° with a negative gain margin. Why does system…
Part Number: SM320C6678-HIREL Other Parts Discussed in Thread: LM10011 Is it mandatory to set CVDD start up voltage to 1.1V,
Because as per my current design
Rset=301k, Rfb1=8.45k, Rfb2=10k
So theoretically calculated CVDD= 1.107 - 0.000507 = 1…
Hi Philly - did you use the LM21215 quickstart tool to verify the stability of your design? If so, please forward. Also, can you send a scope shot of the SW node waveform? Finally, I would like to review your PCB layout. Note that if a SYNC signal isn…
Hi!
I think (as per my calculation) the equation 16 for fz2 on page 21 not correct.
There should be Rc2 instead of Rc1 i.e. fz2 =1/[2.pi .(RC2 + RFB1).CC3].
and the fp2 can be simplified to 1/[2.pi.RC1 CC2) because Cc1 >>Cc2
regards
Bishnu
Part Number: TPS54010 Other Parts Discussed in Thread: LM21215 Dear team,
Only maximum height is specified on the DS , could you please share nominal and tolerance as well as Theta_JC_Top et Theta_JC_Bot ?
Customer is using Two-Resistor Compact…