Other Parts Discussed in Thread: CSD17483F4 , CSD17304Q3 To Whom It May Concern,
SiliconExpert Technologies has been contracted by our customer to work with their suppliers to collect component information (see attached Letter of Authorization). We would…
Part Number: UA78M Other Parts Discussed in Thread: LM2990 Looking for p2p compatible device with below competition.
MC78M12ABDTRKG
MC79M12BDTRKG
application: Servo Motor Drive
Ambient Temp: 125~-40degree
Other Parts Discussed in Thread: LM2990 On LM2990 package, why is it "TAB is Input"?
(Why isn't it "TAB is GND"?)
Other negative linear reg devices, same pattern.
Please let me know a necessary reason of these device.
Best regards…
Other Parts Discussed in Thread: LM2990 I'd like to use long-life hybrid polymer output caps with these regulators. Something like Panasonic ZA series ( http://industrial.panasonic.com/www-data/pdf/ABA0000/ABA0000CE136.pdf ).
I can see from the regulator…
Other Parts Discussed in Thread: LM2990LM2990 Negative LDO - output oscillation question
What we are seeing is ~1Vpp @ ~26KHZ oscillation at the LM2990 output.
When we remove Cout the oscillation persists, but with a different frequency.
Cin and Cout…
Other Parts Discussed in Thread: LM2990 hello, could someone pass me the connection for a source with vout + / -15 and with lm2990 LM2940.
thanks greetings
Other Parts Discussed in Thread: LM2990 Greetings, I'm currently working on a -12V power supply that can output 0.25A of current using the LM2990 -12V fixed output option. I'm plan to input -20V @ 0.3A to the LDO using charge pumps whose output are -Vin…
Hello Danilo
I cannot open the TINA-TI file. Looks like the file is corrupted.
DAP should be connected to the #6 ground pin.
Please do not allow the switching current flows through the DAP of the IC when you layout the board.
Current loop is highlighted…
I need to update these parts in our Approved Supplier List to enable Procurement to purchase them. They were originally listed as National Semiconductor parts, which needs to be changed to TI due to the acquisition. The original manufacturing site is listed…
Other Parts Discussed in Thread: TLV759P , LM2990 Hi!
Can You explain definition some LDO parameters in datasheets? My ask about line and load regulation. Document SLVA079 ( http://www.ti.com/lit/an/slva079/slva079.pdf ) define description for line and load…