Dear George,
1) Attached Adc415.pp.txt is for CCS Ver 4.1.5 Adc415.pp.txt
also building option for CCS version 4.1.5 are
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 'Building target: Hertz_VAF_Meter_29thmarch14.out' 'Invoking: MSP430 Linker' "C:/ti…
Part Number: TMS320F28335 Other Parts Discussed in Thread: C2000WARE
Hi,
I will give preliminary information to describe my problem. I am try to make an embedded system which will upload any program to f28335 mcu over uart serial communication. So…
Xavier,
Can you check to make sure that Device Mode in the ZCG is set to MAC Mode(see page 21 in the attached). This needs to be done to operate on PRIME protocol.
Best,
Matthew tidu237.pdf
Well, I seem to have kind of fixed the issue after installing SYS/BIOS from the Resource Explorer rather than using DSP/Bios (what the difference is, I really don't understand). Using an example from there (clock experimenter kit) seemed to build and…
Hi Sal,
You can see Rev. B of the TRM attached. Newer TRMs should also be okay to use since they are supposed to highlight features that are not available with older versions of the firmware (see the image below for an example).
/cfs-file/__key…
Part Number: AMC1100 Dear TI team,
Good evening.
We are measuring AC voltage of 50KHz switching frequency and fundamental frequency of 50Hz at input side of AMC1100,which is very noisy.(Kindly find the attached images of waveform.doc)
We are not…
Other Parts Discussed in Thread: DP83848C Hello,
I am looking to integrate this part into my design. The pinout table in the march 2015 datasheet calls for a pin 49 for GNDPAD.
This consistent with the Pin Layout Diagram in Section 4.1 and the Package…
Hi Michael,
As you stated previously, this is most likely due to a manufacturing issue. Without knowing the full extent of the issue, we can best conclude that the PCB is not reaching proper temperatures due to thickness of the board, therefore, causing…