Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi Expert,
My customer Bosch is using TAS2505-q1 for quite a long time. We are setting bench to test the THD+N EVM on analog input mode and digital input mode.
Analog Input
I do the test…
Part Number: TLV1822-Q1 Other Parts Discussed in Thread: TLV1822 Hi team,
I am just studying TLV1822 (Open Drain output type comparator)
I have found that if Vin+ >> Vin- , then Vout should be high. it means internal fet should be P Type FET or PNP Transistor…
Part Number: LM4040-N-Q1 Hi Sir,
Why I did not find the operating temperature range for LM4040QCEM3-2.5/NOPB on the datasheet or website?
Could you share the information with me?
Hi Xiaxiang,
Xiaoxiang Liu said: DOUT+ and DOUT- are connected according to the correct cable sequence, but it doesn't work.
Can you clarify what you mean by correct cable sequence?
Please share additional information:
1. Can you share the schematic…
Part Number: LM4050-N-Q1 Other Parts Discussed in Thread: LM4040 , Hi team,
My customer use LM4050 to replace Diodes LM4040.
Input voltage is 6.5V, input resistor is 150 ohm. They connect 2 22uF capacitor at output node.
In Diodes LM 4040's experiment,…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 Hi, I am looking for a solution to drive a N-Channel MOSFET. Use case: I am driving my load using a Battery which is operated from 8V to 24V, and current about 60A. I am looking for solution…
Part Number: TLV840-Q1 Other Parts Discussed in Thread: TLV840 Hi Team,
May I use TLV840-Q1 to achieve below design?
We would like to use – TLV840MADH-Q1: open-drain, active-high and VDD level is 3.3V and 1.8V. I don't find in datasheet. Can you suggest…
Part Number: LM4041-N-Q1 Other Parts Discussed in Thread: REF34-Q1 , REF31-Q1 , REF2025 , INA240
Dear team,
My customer uses our LM4041AIM3-1.2/NOPB, and the temp range is -40-85C. Based on testing, they found that the temp range is too small, and they need…