Part Number: SN74HC4851-Q1 Tool/software: Dear Sirs,
Could you provide the information requested in the beneath table for the P/N SN74HC4851QPWRQ1 please?
Part CTE
PCB CTE
Leadframe Base Material (e.g., copper)
Plating Materials…
Part Number: TDA4AH-Q1 Tool/software: Finishing up layout for board, but need to add the pin delay parameters for the interposer for finalization Where do I get this ?
Part Number: LMV932-N-Q1 Tool/software: Hi Team, I need support in datasheet.I couldn't find max and min operational input voltage levels.I could see only absolute max and min input voltage levels.Please help me to provide details.
Part Number: DS90UB960-Q1 Tool/software: Hi,
My SoC Supports MIPI CSI-2 and I have LVDS Camera. Can I able to interface LVDS camera to my SoC with TI P/N#DS90UB960-Q1. if not, could you please suggest the correct part from TI.
Hi
On the datasheet, it is mentioned as the following,
" This pin must be left floating or connected to pin 2."
Why is it? Is that possible to connect pin 1?
Regards,
Koji Hamamoto
Part Number: DP83TG720S-Q1 Tool/software: Hi,
We connectted DP83TG720S to a switch using SGMII. But we connect RX_P of DP83TG720S to RX_N of switch, RX_N of DP83TG720S to RX_P of switch.
How to change the SGMII P and N? I have set SGMII_CTRL_1 Register…
Part Number: TAS6421-Q1 Other Parts Discussed in Thread: TPA6304-Q1 Tool/software: Hi team,
Does the TAS6421-Q1 have a setting for THD+N similar to the TPA6304-Q1 regarding CLIP?
If not, what is our default clipping THD+N? 10%?
Part Number: TDA4VH-Q1 Tool/software: Customer said In the IBIS model, differential signals like DDR DQS P/N are all inverted, please help to confirm, and if it impact simulation result?
Part Number: DP83TC812S-Q1 Tool/software: Dear TI friends
I submitted a case a month ago, TI specialist told me that t he PHY cannot withstand 16V directly from the battery even if it is shorted at the connector.
case adress:
https://e2e.ti.com…
Part Number: DP83TC812S-Q1 Tool/software: Dear Ti friends,if ethernet connector pin short to battery DC 16V, can TRN_P/N pin withstand this voltate surge?