Part Number: LM4050QML-SP Are the unused pins (1-4, 6-9) on the LM4050QML-SP connected to anything internally?
Looking at an application where two LM4050 references will be stacked to double the reference voltage. Basically, pin 5 of the upper Ref will…
Part Number: LM4050QML-SP Hi,
I would like to ask if TI is able to provide 5962R0923561VZA (LM4050QML-SP), with a lower sceening. It should withstand thermal cycling and vibration. Intention is to build prototype before moving to flight ready models…
Part Number: LM4050QML-SP Hi,
I would like to know if the ELDRS and SET tests indicated on the TI website ( LM4050WG2.5RLQV ELDRS Characterization Report Data, LM4050WG5.0RLQV ELDRS Report and LM4050WG2.5RLQV SET Report dated 11 May 2012) are still valid…
Hi Oscar,
There seems to be a bug in our E2E Forum site because I can't find this post a few minutes after posting so I created another one in the link below. You will noticed that there is a 30min time difference between the two post. Anyway, thank…
Hi Kevin,
For rad-hard 2.5V references, there are a few options: t he LM136A-2.5QML-SP , the 2.5V option of the LM4050QML-SP , and the TL1431-SP . All of these parts do have TID reports (sometimes referred to as ELDRS reports for older documents) available…
Part Number: DAC121S101QML-SP Other Parts Discussed in Thread: LM4050QML-SP Hi Team,
My customer is looking at using the DAC121S101QML-SP for an application that requires low 1/f noise, in the 0.1 - 10Hz range. This part would likely be fed by a LM4050QML…
Part Number: TPS7A4501-SP Other Parts Discussed in Thread: LM2940QML-SP , LM4050QML-SP My customer is looking for a QML space-rated voltage regulator that can survive 50Krad, has SET and SEE testing, an input voltage of 10V minimum, and an output of 5V…