Part Number: LM5155-Q1 Other Parts Discussed in Thread: UCC28C43 , LM5155 Hi all,
Customer want to use LM5155 like UCC28C43, can they short FB to GND and connect comp to opto-isolator output? Thanks.
Part Number: LM3478 Other Parts Discussed in Thread: LM5155 Tool/software: Hi,
Q1. I believe that the variation in V_SENSE and V_SL ratio described in the Electrical Characteristics of the data sheet is temperature dependent, is this correct? Also, are…
Hello Jimmy
LTC3704 is boost controller which is configured for SEPEIC topology. Please check LM5155 at https://www.ti.com/lit/ds/symlink/lm5155-q1.pdf .
-EL
Part Number: LM5155-Q1 Other Parts Discussed in Thread: LM5155 Team, can you please help answer my customer's question:
We have the typical circuit from the datasheet implemented. With no input voltage going into the BIAS line (cut trace) I still see…
Part Number: LM5155-Q1 Tool/software: WEBENCH® Design Tools Hi,
I'm fairly new with boost converter and I don't understand why, I have such a difference between Vout Actual and Vout when I look in Webench report. My parameters are the followings:…
Part Number: LM5155-Q1 Other Parts Discussed in Thread: LM5155 , UCC24612 , PMP22151 , PMP40569 Hi Team,
My customer is finding the isolated DC/DC solution and below is the spec.
Vin = 13V-36V (nominal = 24V)
Vout = 24V
Iout = 4A
I find that LM5155-Q1 could…
Part Number: LM5155-Q1 Other Parts Discussed in Thread: LM5155 Hi Team,
I have questions about UVLO/SYNC pin specifications as below.
1. Do we have any spec for current flow at UVLO/SYNC pin? I can only find <1mA recommendation when UVLO/SYNC pin is…
Part Number: LM34966-Q1 Other Parts Discussed in Thread: LM5155 , UCC28600 , TPS92210 I have a application with the input condition from 9V~16V and output with 60V/0.6A. And isolation is needed, is there some AHB solution for this?
if not, is there some…
Part Number: LM51551-Q1 Hello,
By looking at bode plot, am I getting phase margin around 61deg? Is the phase margin plotted by quick start calculator accurate?
Is it ok to assume