Part Number: LMH0302 Hello,
The datasheet says theres is an internal pull up resistor on ENABLE pin. What is the minimum and maximum resistor value?
Moreover, what is the input leakage current of SD_HD input pin please?
Thanks
Part Number: LMH0302 HI,
My customer has the following questions:
The input capacitors on the LMH0302SQE/NOPB device and output filtering is different than the data sheet recommendations.
The ac coupling input capacitors are 0.47 uF rather than the suggested…
Hi Amy,
1). Complete 10 bits need to be provided to the LMH0030 device. 10-bits X 27MHz is equivalent to 270MBps.
2). 10 Bits at 27MHz clock can be used to meet these two requirements.
3). Typically FPGA along with a serializer is used. There are two…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH0302 LMH0324 configuration parameters are as follows
0x00=0x08
0x27=0x04
0x30=0xA3
0x31=0x63
0x32=0x00
0x33=0x00
Part Number: LMH0302 Other Parts Discussed in Thread: LMH0307 , LMH0324 Hi Team,
My customer want to use LMH0302/LMH0307 as a 3G SDI cable driver. The distance of the cable may be about 50m. Can you help check the drive capability of these two devices…
Part Number: LMH0302 My customer is using the LMH0302 to drive a 3G-SDI signal to a BNC connector that mates directly the the chassis. Therefore, the BNC connector is mated to the Chassis ground.
In Figure6 (p.11) - "Layout Example" in the LMH0302 datasheet…
Part Number: LMH0394 Other Parts Discussed in Thread: TS3USB221 , LMH0302 , LMH0387 , LMH0397 , DS25CP102 Hi team,
My customer is using LMH0394 in RX and LMH0302 in TX for SDI application. But now they want to put TS3USB221 before LMH0394/LMH0302 as a TX…
Part Number: LMH0302 Hi!
In some schematic i have Rref 75 Ohm instead recommended 750 Ohm. May this situation cause the permanent damage of the device?
Other Parts Discussed in Thread: LMH0344 , LMH0356 , LMH0302 , LMH0346 Dear Team,
Please share me the eye pattern requirement for below ICs.
1)LMH0344SQ/NOPB
2)LMH0302SQE/NOPB
3)LMH0346MH/NOPB
Also share me Ibis AMI model for above parts.also (.ami and .dll…
Other Parts Discussed in Thread: LMH0302 Hello,
My customer as the following issue,
Could you please give him support ?
Hello, I am trying to use the LMH0302 with a single-ended input as opposed to a differential input. The datasheet says this is possible…