Part Number: LMH0303 Dears
We are using LMH0303 in our equipment. I observed the waveforms when the power of the device was turned on and off. I found ringing in the middle of the rising/falling waveform of the RREF pin. What is the possible cause?
Also…
Part Number: LMH0303 Other Parts Discussed in Thread: DS30BA101 , DS30EA101 , Dear staff,
I have a question related to the SDO video output.
Question 1
How I can set the SDO as the 100ohms differential twisted pair to pass through a highspeed connector,…
Part Number: LMH0303 I'm considering the use of LMH0303 and examining its characteristics by simulating it using the IBIS model available on your website.
The IBIS model simulation circuit was created at 2.97 Gbps and the output waveforms were checked…
Part Number: LMH0303 Dears.
I have three questions.
Question 1 Will the LMH0303 FAULT signal (PIN 13) can be LOW if the SDI signal (PIN1 PIN2) can not be received?
Question 2 My system is looking at the FAULT signal (PIN 13) of LMH0303. If the FAULT signal…
Part Number: LMH0303 HI Team.
i found below description in datasheet 7.3.5. So if we want to enable the cable detection function, we need to pull-up the enable pin firstly, right? And if we pulled-down the enable pin, the cable detection function can…
Part Number: LMH0303 Dears
We are using LMH0303. The LMH0303 datasheet shows the typcal of jitter. Can you tell me the worst jitter value (Max) of 2.97 Gbps/1.485 Gbps?
Sincerely,
Part Number: LMH0303 HI Team,
Can LMH0303 support ST344?
I see the first page of datasheet mentions the ST344. But there is no details to introduce how to set up for ST344. Please help to confirm. Thanks.
Part Number: LMH0303 Hi team,
If you have an open / short test report for future development, please provide it.
(Short to adjacent pin, short to GND, short to supply, and each pin is open)
Orderable Device : LMH0303SQ/NOPB
Regards,
Hitoshi Koide
Part Number: LMH0303 Dears
I output 3G-SDI from a xilinx kintex lutrascale transceiver and input it to LMH0303. I'm thinking of driving with LMH0303.
I'm thinking of AC-coupled the interface with LMH0303 at 4.7uF, is that OK?
Sincerely,
fig…