Part Number: LMH0303 Dears
I output 3G-SDI from a xilinx kintex lutrascale transceiver and input it to LMH0303. I'm thinking of driving with LMH0303.
I'm thinking of AC-coupled the interface with LMH0303 at 4.7uF, is that OK?
Sincerely,
fig…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0397 , LMH0318 Hi.
I have two questions.
Q1
I want to improve the rising waveform.
Is there a register that can improve waveform?
Q2
Is the amplitude of the waveform improved with register 0x4 AMP…
Part Number: LMH0303 Hi.
I want to confirm a circut.
My design has one output port. So it does not have two output port.
I will attach the design I thought.
Is there a problem with this design?
Sincerely, design.xlsx
Part Number: LMH0303 Other Parts Discussed in Thread: DS25CP152 , Can the DS25CP152 MUX be used to drive a LMH0303? What interface connections are needed to meet the common-mode voltages?
Is it the same as described in this posting?
https://e2e.ti.com…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0302 Hi team,
I have a question about the LMH0303 SDI cable driver. It has worked very well for my customer to drive a 75 ohm single ended coax cable. My question is, can it be used to drive an…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0302 Hi Team,
When the resistors in the red box are not connected, the AC coupled input signal can be detected, why can the AC input signal be detected by doing so.
However, when the resistors are…
Part Number: LMH0303 Hi,
I use the LMH0303 for cable driver of Xilinx Spartan6 GTP TX.
When I check the "Figure 5 shows the application circuit for the LMH0303." in the LMH0303 datasheet I saw it can have two SDI output.
1. Can anyone explain…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0318 Hi team:
my application is below,the pcb is FR4,my question is :what is the max length between FPGA and LMH0303 can be routed?
thanks