Part Number: LMH7322 Tool/software: Hello team,
Would it be possible to give me deterministic jitter performance for LMH7322? (Fixed clock input) The datasheet only shows random jitter performance.
My customer would like to use this device for clock…
Part Number: LMH7322 Tool/software: Hi
We are using LMH7322 comparator to compare two analog inputs in one of our new design.
The LMH7322 output will be LVDS signal which will be interfaced with a 2.5V LVDS receiver.
As termination requirement is not…
Part Number: LMH7322
Tool/software:
Hello team,
Does LMH7322 accept AC-coupled signal input, when the device is operating in single supply? (VCC=3.3V, VEE=0V)
Sould I set the common-mode voltage to (VCC-VEE)/2?
Best Regards, Kei Kuwahara
Part Number: LMK04832 Other Parts Discussed in Thread: LMH7322 ,
Tool/software:
Hello team,
My customer wants to clean jitter from the output of LMH7322, whose jitter is 572fs or even worse in condition. Below is EC table from LMH7322.
Would it…
Part Number: LMH7322 Other Parts Discussed in Thread: CDCLVP111 , Tool/software: Hello team,
My customer is trying to convert 4.2Vpp clock to LVPECL clock for CDCLVP111.
Is LMH7322 capable of 4.2Vpp input clock? I am worried because VRID is only …
Part Number: LMH7322 Tool/software: Hi, and thanks for reading this!
I have a PCB where a custom chip produces four LVCMOS 1.2V outputs - named OUT_0, OUT_1, OUT_2, OUT_3 - which I had to convert to LVDS. I considered implementing two LMH7322SQ/NOPB…
Part Number: LMH7322 Tool/software: I am using LMH7322 as the vcci to be a 12v and want to reduce the vcco values such that the total output of the device is 3.3 in high and 2.8 in low , is that possible ? and what is the maximum voltage difference between…
Part Number: LMH7322 Other Parts Discussed in Thread: TLV1805 , TLV3801 , TLV3604 , TLV3605 Hi,
I am looking at LMH7322 comparator for triggering scope with the following :
1.Input voltage range of 80V..Not sure if LMH7322 handles that scale..
2…
Part Number: LMH7322 Other Parts Discussed in Thread: TINA-TI , I downloaded PSPICE model from https://www.ti.com/product/LMH7322 and am having errors when running using ORCAD 17.2.
.SUBCKT AND2_BASIC_GEN_SAN_0 IN1 IN2 Y PARAMS: VDD=1 VEE=0 VTH=0…
Part Number: LMH7322 Dear TI team: Can LMH7322 used for negative signals?
Customer want to choose a comparator to replace MAX9600, it can used for negative signals application, and also need low power consumption.
Thanks!
Regards!
Eric Shen