Part Number: LMT01-Q1 Other Parts Discussed in Thread: LMT01 , LMT01EVM Tool/software: TI C/C++ Compiler How to design mcu’ program for reading temperature of LMT01-Q1?(C language)
Is there a sample program?
Part Number: LMT01-Q1 Other Parts Discussed in Thread: LMT01 Hi,
On the datasheet it states: "Alternatively, the LMT01-Q1 can be mounted inside a sealed-end metal tube, and then can be dipped into a bath" Could you please give me a bit more information…
Part Number: LMT01-Q1 Other Parts Discussed in Thread: LMT01
Hi team,
The customer uses LMT01-Q1. He also uses SOT-92 package.
When the air temperature is 20℃, LMT01-Q1 can output 1120 pulses. But when LMT01-Q1 is in -1℃ for 2 minutes, the number…
Part Number: TMS320F280049C-Q1 Other Parts Discussed in Thread: LMT01 , LMT01-Q1 Hi,
I need to do some temperature measurements in a high noise environment where an NTC just wont do. And it needs to be small, cheap and automotive qualified...because…
Part Number: LMT01-Q1 Hi guys,
can you comment on how robust against disturbances is the digital interface of LMT01-Q1 for long distance communication (~1mt) between sensor and microncontroller, compared to a regular NTC with analog output?
Regards…
Part Number: LMT01-Q1 Other Parts Discussed in Thread: LMT01 Different configuration is shown for the device.
VN pin directly connected to ground.
Is this configuration is OK.
Part Number: LMT01-Q1 Other Parts Discussed in Thread: LMT01 Hi, Team,
We have a question for the reliability report. Can we ensure the accuracy for the LMT01 after the reliability test? We only saw it pass the test, not should whether the accuracy…
Hello,
Below the answers...
General: A heat meter is basically a flow meter that also measures the temperature of the forward flowing medium towards the heat exchanger and back flowing medium away from the heat exchanger. The medium is usually water…
Are you mainly interested in high-accuracy sensors? The Q1 denotes automotive qualification, which doesn't seem relevant to your application. You could use the regular TMP275 instead.
Other high accuracy sensors:
Part Number
Description
…