Part Number: TLV1822-Q1 Other Parts Discussed in Thread: TLV1822 Hi team,
I am just studying TLV1822 (Open Drain output type comparator)
I have found that if Vin+ >> Vin- , then Vout should be high. it means internal fet should be P Type FET or PNP Transistor…
Part Number: LM4040-N-Q1 Hi Sir,
Why I did not find the operating temperature range for LM4040QCEM3-2.5/NOPB on the datasheet or website?
Could you share the information with me?
Part Number: LM4041-N-Q1 I am using LM4041QEEM3-1.2/NO regulator to get 1.2 volt output. But when checked it with no load condition it's giving me 1.4 Volt output an with 15 mA load it is giving me 0.8 Volt output. My Rs value is 47 ohm. Please suggest…
Hi Xiaxiang,
Xiaoxiang Liu said: DOUT+ and DOUT- are connected according to the correct cable sequence, but it doesn't work.
Can you clarify what you mean by correct cable sequence?
Please share additional information:
1. Can you share the schematic…
Part Number: LM4050-N-Q1 Other Parts Discussed in Thread: LM4040 , Hi team,
My customer use LM4050 to replace Diodes LM4040.
Input voltage is 6.5V, input resistor is 150 ohm. They connect 2 22uF capacitor at output node.
In Diodes LM 4040's experiment,…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 Hi, I am looking for a solution to drive a N-Channel MOSFET. Use case: I am driving my load using a Battery which is operated from 8V to 24V, and current about 60A. I am looking for solution…
Part Number: TLV840-Q1 Other Parts Discussed in Thread: TLV840 Hi Team,
May I use TLV840-Q1 to achieve below design?
We would like to use – TLV840MADH-Q1: open-drain, active-high and VDD level is 3.3V and 1.8V. I don't find in datasheet. Can you suggest…
Part Number: LP38691-Q1 Other Parts Discussed in Thread: LP38691 Hi TI expert,
May I know whether I can directly replace LP38691SD-5.0/NOPB with LP38691 Q SDX-5.0/NOPB ?
And how to identify whether LP38691QSDX-5.0/NOPB is qualified as AEC-Q100?
Or all solution…
Part Number: LM74501-Q1 Other Parts Discussed in Thread: LM74502-Q1 Dear TI team,
I am planning to replace P-Ch MOSFET based High Side Load Switch with N-Ch MOSFET + HS Driver IC. Load current is 10Adc/60Vdc. Reverese polarity protection is not required…