Part Number: LSF0108-Q1 Tool/software: Linux Hi, I'd like to know the correct usage of LSF0108-Q1.
The datasheet indicates the LSF0108-Q1's ENABLE pin should be connected to filter capacitor between GND but example capacitance is not mentioned.
Could…
Part Number: LSF0108-Q1 Hi team,
A-side High level voltage is higher than Vref_A.
The datasheet figure also appears to be higher than 1.8V.
Could you provide me the reason?
If this cannot be avoided, what is the voltage range?
Best regards,
Tomoaki…
Part Number: LSF0108-Q1 Other Parts Discussed in Thread: SN74LVC1G07 Hi team,
If the low-side A power supply terminal is open, is the internal reference MOS gate fixed to the high-side B voltage?
The general connection is as follows.
I think that Vccb…
Part Number: LSF0108-Q1 Team,
Does the LSF0108-q1 translator have a simple FET internally? If so, I’m a little confused how the FET turns on for down-translation vs up-translation. Watching the training videos, the body diode of the FET doesn’t seem to…
Part Number: LSF0108-Q1 Hi team,
We want to minimize the pull-up resistance in the following figure.
We want to make resistance as small as possible from the viewpoint of immunity.
I want to make it 10kΩ if possible.
Is that possible?
If it is…
Part Number: LSF0108-Q1 Hi team,
For LSF0108-Q1, it seems that there is no spec of VIL/VOL in datasheet. Is there any reason not having the spce?
Can you let me know the spec for each voltage?
Thanks,
Sam Lee
Part Number: LSF0108-Q1 Hello
we have some questions , could you tell us about below?
1:
according to the datasheet "9.2.1.2.1" , it described "the EN input must be connected to Vref_B and both pins pulled to HIGH side Vpu through a pull-up resistor…
Part Number: LSF0108 Other Parts Discussed in Thread: TXU0104 , SN74AXC4T774 , SN74LV126A , SN74LXC8T245 , SN74LV125A , SN74LXC8T245-Q1 , Hi,
We are planning to use LSF0108QPWRQ1 for bidirectional GPIOs of our processor board, wherein each line can be configured…
Part Number: LSF0108-Q1 Other Parts Discussed in Thread: LSF0108 Hello,
I would like to know how to calculate the power dissipation of LSF0108-Q1 ??
Best Regards
Rana
Part Number: LSF0108-Q1 I need automotive qualified >6-bit 3.3V to 5V level translator. Could you please share brief comparison between LSF / TXS / TXB series translators ?