Hi Board designers,
Refer below inputs for the OLDI interface related queries.
AM620-Q1 does not support OLDI interface.
Supported display configurations.
Does AM62xx support 4 lane or 8 lane or both 4/8 lane type of LCD displays.
The AM62x…
Part Number: LMK04828 Other Parts Discussed in Thread: LMK04832 Hello,
We are working on the xilinx based RFSoC application Design and planning to use LMK04828B for reference clock
As per our understanding from the LMK04828B datasheet, the output…
Part Number: DS90UB949-Q1 Hello team, I am using a DS90UB949-Q1-based EVK kit for my test. My setup is such that, I have a device present at the Deser (UB948) side which is connected to the Deser using I2C and a GPIO pin is also input to the Deser. The…
Part Number: DS90C187
Hi Team, customer uses TI DS90C187LFX (Digital RGB to LVDS). Customer set pin 18B to high (18bits). it has abnormal display. it should be 16 gray scale.
Any suggestion for the abnormal case?
Here is the normal and abnormal…
Part Number: MMWAVEICBOOST Other Parts Discussed in Thread: IWR6843ISK The current interface to the LVDS of the MMWAVEICBOOST + IWR6843ISK goes to a DCA1000 board and uses a Lattice Semi FPGA for processing data. However, for our application, the speed…
Part Number: TMUXHS4212 Other Parts Discussed in Thread: HD3SS3212 Hi,
We have a system where we have to connect a ZynQ ultrasclae EVK to 6 nos of Spartan 6 FPGA through asynchronous LVDS (Tx&Rx) running at 100 Mbps (50MHz), DC coupling mode ( no ac…
Part Number: TDA2 Tool/software: Linux Hi Sir,
My HW is TDA2x CPU board + Vision Board + daughter board + LVDS sensor and SDK is PROCESSOR_SDK_VISION_03_04_00_00 with TDA2XX_EVM_LINUX_ALL define.
I select use-case "4CH VIP LVDS capture + SGX MOSAIC…
Hi Jackson,
Thanks for your reply.
If you can run this code and flash to the EVM system with no problems, then it seems that a difference between this and your customer HW might be an issue. Are there any major differences in the HW setup?
==…
Part Number: SN65DSI84-Q1 Other Parts Discussed in Thread: SN65DSI84 , DSI-TUNER Tool/software: Linux Hi,
We are using SN65DSI84 in our hardware and we have implemented a MIPI to LVDS converter using this chip set. First we tested the video pattern…
Hi Brian,
Can you check all jumpers at default setting on both EVK boards? Can you send me a list of settings? What happens if you remove all input data and only provide a clock? Can you probe the input clock and see what the signal quality is.
…