Part Number: DS92LX1621 Other Parts Discussed in Thread: DS92LX1622 , , LX16EVK01 Hello all,
we are designing an equipment where we plan to move data between two board using ser/des pair DS92LX1621 / DS92LX1622.
The distance between boards is rouglhlty…
Hi Martin,
You can buy the EVM kit here: www.ti.com/.../lx16evk01
but there is no option to buy it with just the serializer. It comes with both serializer and deserializer.
Regards,
I.K.
Part Number: DS92LX1621 Other Parts Discussed in Thread: LX16EVK01 We are using the evaluation kit LX16EVK01 to test some cable and we need to layout a different board to work with the LX16EVK01 board. Just wondering if we can have the pcb gerber file…
Other Parts Discussed in Thread: DS92LX1622 , DS92LX1621 , LX16EVK01 , DS91C176EVK Hi,
I got the Evaluation Board LX16EVK01 with the Serdes DS92LX1621 and DS92LX1622.
I used the following DIP switch settings:
DS92LX1621: RESO = LOW
M_S = LOW …
Hi Dac,
It just seems odd that the designer of the LX16EVK01 constrained the usage of Y1 to 1.8V only. I should think users of the board might wish to use a local oscillator with 1.8 as well as 3.3 voltage levels. I don't know why you are saying that…
Other Parts Discussed in Thread: DS92LX1621 , LX16EVK01 Hello,
I tried to measure the cml-signal between the serializer and deserializer. I have got a squarewave signal which is modulated on another signal (see attached pictures)
Is this carrier signal…
Hi Dac,
the result of the measurement with the DES pcb standalone shows register 0x1F = 04. The voltage at the mode pin is 0.94 V.
We don't use the SERDESUB-913ROS evaluation board. We did our development with the LX16EVK01 EVM snlu013 evaluation kit…
Junqiang Shi said: what is the ch3/ch4 in the plot? it is the channel link (Dout+-/Rin+-)
I was using 1621 with internal CLOCK source, I changed it to external PCLK=40Mhz and Now LOCK and PASS pins are High, and it seems to work.
I drive DIN(0-15) pins…