Part Number: J784S4XEVM Other Parts Discussed in Thread: PCM3168A Tool/software: Hi, We have updated to SDK 10.1 and are encountering several GStreamer pipeline issues. These same pipelines functioned correctly under SDK 10 1. Following pipeline just…
Part Number: CC2640 Other Parts Discussed in Thread: CC2592 , CC2650
Hi Team,
customer has some question, please kindly support it.
thanks!!!
Hello, during the process of using CC2640F128RHB, we found that the signal transmission distance of…
I'm not aware of any Ti code that includes a USB host API and I hope someone responds that does. The following approach is straight forward and well proven.
The SmartRF04 uses a SiLabs C8051F320 (F320) which has the USB function used to communicate…
Chuck,
i will try to answer your questions inline so I don't miss one:
I understood from your previous answers that TRM Table 4-1 (144-pin package) is useful ONLY for the configuration of the listed terminals as inputs, and Table 4-16 (for both 144…
Sorry if I answear just now but i've been away.
My LPM3 testing code it's the same as the LPM4 cose except for __bis_SR_register(LPM3_bits);
As you suggest (thanks!) I connected ACLK to VLO
UCSCTL4 &= 0xF8FF;
UCSCTL4 |= SELA__VLOCLK;
and…
Part Number: TDA4VM Hi TI members:
I also meet the questions same as thread
root@j7-evm:~# source /opt/vision_apps/vision_apps_init.sh root@j7-evm:~# APP_LOG: Mapping 0xb8000000 ... APP_LOG: Mapped 0xb8000000 -> (nil) of size 262144 bytes APP_LOG…
Part Number: TPS65982 Other Parts Discussed in Thread: TIDA-01243 , TPS65987D , TPS65988 , Hello Guys,
I had posted article about my current project. But there was no active comment..
So I posted it again.
I assembled this pcb, and get nothing…
Hi Gilbert
There were several changes going from SPRUH77a to 77b
I am sharing the revision history log
Changes from December 1, 2011 to July 10, 2016 (from A Revision (December 2011) to B Revision)
I have attached the entire pdf.
The changes…
Other Parts Discussed in Thread: TMS320C5505
Hi,
I have a problem
getting two tasks to co-exist properly on a VC5505 patform, using the CCSV4
tools with the following environment…
Processor: 320VC5505
@ 100MHz.
…