Other Parts Discussed in Thread: CC2520 , Z-STACK Hi there,
I just have a quick question, will the CC2520EM work with my MSP-EXP430FG4618? I have done a bit of reading and have the impression that I can't, however I am still hoping that I can...
…
Hi Derek
Thanks for providing great information for configuring eZ430-RF2500.
I am trying to do this with Code Composer Version: 4.0.2.01003.
I have done everything that you advise but get stuck in Project->Properties->C/C++ Build->MSP430Compiler-…
I just got this board and have been going trough the code examples in the collateral files. All are working with the exception of the Voice Recorder. I've had to make minor changes in some cases. (Does LCDMEM[0] really refer to LCDMEM1 ? That's weird…
I would like to use p6.0 to p6.7 for diffrent usage (header H8).
what should I do?
can it done with out soldering out some reg/cap
or I should solder out those (attached picture).
mic - r29,r30,r32,c21
LPF - r24,r25,c16,c17
jack - r22
is it…
I would like to use p6.0 to p6.7 for diffrent usage (header H8).
what should I do?
can it done with out soldering out some reg/cap
or I should solder out those (attached picture).
mic - r29,r30,r32,c21
LPF - r24,r25,c16,c17
jack - r22
is it easy…
Other Parts Discussed in Thread: MSP430F2013 , MSP430FG4618 can I use the eZ430-F2013 as jtag for the MSP-EXP430FG4618 Experimenter Board
how it can be done
which setting is needed
thanks
I'm supposing you're talking about the MSP-EXP430FG4618.
Use the debugger to look at the two bytes at 0x10FE. My guess is that they're both 0xFF, meaning that InfoA has been erased. This can result from an over-eager code downloader ("Properties…
Other Parts Discussed in Thread: ADS1298 Dear sir,
can i connect msp-exp430fg4618 experiment board to ads 1298 front end board for ecg applications. Please help me in this regard to finalize my design.
Thank you
Dear Sirs,
I'm trying to printf to LCD, modifying the original TI's example for LCD from slac129a.zip
As told in IAR's help, I've added own version of write.c file to my project and customized it as follows:
#include <LCD.h>
…
Hi,
I am working on the MSP-EXP430FG4618 kit and I developed code for UART communication with the hyperterminal of my PC. The communication was going smooth but it has suddenly stopped and I dont know the reason for the same. The receive is happening…