Thanks for your reply.
I am thinkning about MSP-TS430DA38 is it suitable to use with the VQFN 40 pin MSP430FR5959?
Also I have another question regarding MSP430FR5969 VQFN 7mX7m ic , can desolder it from the laucnch pad and solder it in the PCB without…
It is the MSP-TS430dA38 target board. I have tried to reposition JP4-JP9 to pins 1 and 2, but when I try to compile my code on to the MSP, CCS doesn't recognize that the MSP is connected
Here is the link to the target board.
www.ti.com/.../msp-ts430da38
I will see if I can get this linked properly to the -EP datasheet.
If this answers your question, please click "Verify it as the answer"
Regards,
Wade
Hi Aditya Prabhu12,
If you need an "Evaluation Platform" or EVM depends pretty much on how you imagine your development process. An EVM is a good choice if you want to do prototyping (e.g. by wiring up the EVM with a breadboard) and being able to easily…
Part Number: MSP430F2274 Other Parts Discussed in Thread: MSP-TS430DA38 Have 2 cards with MSP430F2274’s, one using UCB0 as an I2C Master reading selected data from an identical card needing to be a Slave. Slave UCB0 code appears to respond, but does not…
Hello Sean,
Using an eZ430-RF2500 with CCS v8.0.0, I can program the code that I shared earlier, open a terminal on the MSP430 Application UART COM port, type a "u", and see "Hello World" printed in the terminal. The only other thing that I think could…
Part Number: MSP430G2955 Other Parts Discussed in Thread: MSP-TS430DA38 Hello.
I have a question.
Is there a way to reduce the current consumption of my code while observing the following conditions?
MCLK = 500KHz
MCLK sourced from 4MHz crystal
VCC…
Part Number: MSP430F2274 Other Parts Discussed in Thread: MSP-FET I have been trying to run the basic example UART code for echoing a received character. However, whenever I open a terminal in CCS and try to type a character nothing happens. I have tried…
Penny, There is no LaunchPad available for MSP430G2x44 or MSP430G2xx5 devices, you will need to use a MSP-TS430DA38 target board and TSSOP38 package and sky-wire to the MSP-EXP430G2 headers on the TPS23861EVM-612 accordingly. Regards, Ryan
Other Parts Discussed in Thread: MSP430G2955 , MSP-TS430DA38 Hello, I'm using a MSP430G2955 in a MSP-TS430DA38 with a 32.768 crystal. I have the program using the using the using the crystal to generate the ACLK and the DCO generating the MCLK and SMCLK…