Part Number: MSP430F1611 Hello ,
I am trying a simple master transmit code as below. I am not able to see the clock signals on the Logic Analyzer. Could someone please tell me what is wrong with the code?
#include "io430.h"
unsigned char TxData…
Part Number: MSP430F1611 I am using MSP430F1611, and I want to perform SPI communication between MSP430F1611(Master) and FPGA(Slave), I can send data successfully from MSP430F1611 to FPGA and get miso data in U0RXBUF and RXBUF0, now problem is how to…
Part Number: MSP430F1611 Tool/software: Code Composer Studio Hi,
We have an old ccs project running on CCS5.4.0.00091_win32, it's compiling successfully, when we imported it to the new ccs version CCS10.0.0.00010_win64, it gives lots of error 1 issues…
Part Number: MSP430F1611 Other Parts Discussed in Thread: MSP430F5324 , MSP430G2553 Hi, I want to communicate the MSP430F1611 with any other controller (e.g Arduino ) or other MSP430F1611 using SPI communication, I visited this ( gist.github.com/.../3326502…
Part Number: MSP430F1611 Hello,
I am trying to use the USART0 for I2C communication and USART1 for UART communication simultaneously in a MSP430F1611 microcontroller. I2C and UART independently works fine, but when i try to configure both at the same…
Part Number: MSP430F1611 Hi,
Background
An existing design had the XT2 crystal changed to adjust the clock frequency and units began no longer being able to start the crystal. Upon review, the load caps were adjusted slightly to account for trace capacitance…
Part Number: MSP430F1611 Other Parts Discussed in Thread: MSP430FR2355 , MSP430FR5969 , MSP430F5529 Hello,
I am fairly new to the MSP family and am starting a project off. I have used the c2000 launch pads and was wondering if there is one for the MSP430F1611…
Part Number: MSP430F1611 Tool/software: Code Composer Studio i want to capture module but it doesn't work
in compere i am getting interrupt but when i switch to capture mode it doesn't going in isr.
i am using hardware multiplier in my project it is working fine for integer number but when i am using it for floating multiplication it is not working correctly
for example when i multiply 2.5*2 it will give result 4 instead of 5 .
is hardware multiplier…
hi
in our project we have to measure and display the voltage of sine wave only when it is in range consider channel frequency is 1.7khz then it has to show voltage only when the input signal is in range of 1.65 khz to 1.75khz for 1.7khz channel otherwise…