Part Number: MSP430F168 Other Parts Discussed in Thread: TMP100 , PCF8574 , DAC8571 Dear sir,
In I2C we are fessing some problems (100KHz only)
ie . 1. some PCB's working properly and some PCB's it is not working and in not working pcb if we connect…
I do not know how to use CCS. I heard that inline assembly does not work. If you do use that, you need to inspect what object code CCS generated.
I think you can use pointers in c to directly do what you intended. No need to do inline assembly.
…
Other Parts Discussed in Thread: MSP430F168 Hi! I'm trying to communicate with the msp430f168 through the bootloader but i can't.
I've checked the signals going out of my computer like test and reset which are the ones that activate the bootloader…
I don't recognize all these version numbers ...
Kenji Totsuka said:
For reference, the versions are the followings.
New compiler/linker from binutils: 5.2.0/2.25.1
Old compiler/linker from binutils: 4.6.3/2.21.1
So I would appreciate if you…
Other Parts Discussed in Thread: MSP430F5336 , MSP430F168 We have two MSP-FET430UIF one hardware 1.3 and 1.4, both firmware upgraded and both work MSP430F168 devices, only the 1.4 works with the MSP430F5336. We have two MSP-GANG, both work with MSP430F168…
Bhal Tulpule said:
I am using a MSP430F168 processor (Master) to download code into another MSP430F168 (Slave) via the BSL ... when I issue a command from the PC via an HyperTerminal on UART0, ...
So you have a F168 as a Master , another F168 as…
Other Parts Discussed in Thread: MSP430F168 , MSP430F5310 Hi,
This is regarding the msp430f168 and I'm using Code Composer Studio 5.1.1.
I need to get my code start at the start address of the flash, in my case 0x4000. In other words, I need my reset…
Other Parts Discussed in Thread: MSP430F168 , MSP430F5419 Hi,
We are writing code for the MSP430F5419 and the MSP430F168, currently we are using CCE v3.1 SR1 but have recently purchased CCS v4.
Can CCS v4 be installed alongside CCE v3.1 or do we…
Other Parts Discussed in Thread: MSP430F168 Hi,
I'm using CCE V3 to write code for an MSP430F168.
Is there a way to have user generated warnings when compiling code something like,
#ifdef SEND_DEBUG_DATA
#warning "Sending Debug Data"
#endif…
Other Parts Discussed in Thread: MSP430F168 Hi,
I'm writing code for an MSP430F168.
Are there status bits that can be inspected on start-up to determine why we have reset i.e. POR, BOR, watchdog timeout etc?
Thanks,
Ben