When I installed CCS I did install it in a separate folder....."C:/TI"
When I build the project these are the errors I got.........
'Building target: exa.out'
'Invoking: Linker'
"C:/Ti/ccsv4/tools/compiler/msp430/bin/cl430…
Other Parts Discussed in Thread: MSP430F2417 , TMS320F28334 Hello,
I find a solution to reprogramme my msp430f2417 by usb.
In my board i use ft2232 for reprogram my tms320f28334.
It's possible to use a second port of ft2232 to reprogram my msp430f241…
Other Parts Discussed in Thread: MSP430F2417 I have read the application note on interfacing 5V circuits to 3V MSP430s and know that I want to use a resistor divider to interface my 5V current sense amplifier to the MSP430 running at 3.3V. I will likely…
slau144e.pdf is not the most recent version. But anyway, at the bottom of each page, there is a link to "Submit Documentation Feedback". Do not expect a reply, but they do listen.
Yes, they use BARx as a short-hand for BAR0, BAR1, BAR2, BAR3…
Other Parts Discussed in Thread: MSP430F2417 hi,
how can I make UART of MSP430F2417 to print the characters that I provide through uart , that means It should print the characters that i provide through terminal (hyperterminal)
Rupesh
IIT kanpur
Other Parts Discussed in Thread: MSP430F2417 Hello everyone,
I am using a MSP430F2417 device and CCE. I am working on a code with extensive floating point calculations. The floating point arithmetic calculation routines in the run time support library…
Hi there,
Thanks for the reply.
By "unusually long time" I meant that the code execution on the MSP430F2417 was quite long as compared to the MCS51 architecture processors. Actually I am trying to port a code from a 8051 based controller to the…
Other Parts Discussed in Thread: MSP430F2417
Hi all,
I have a question regarding the RAM memory of the MSP430F2417, because it seems that I am not able to use the whole 8Kb RAM memory space but only around half of it. I am using IAR Embedded Workbench…
Other Parts Discussed in Thread: MSP430F2417 My old laptop just gave out so I just bought a new laptop and installed code composer (4.1.1.00014). Whenever I try and debug my project I get the following error message: Warning: CPU is OFF and further debugging…
Other Parts Discussed in Thread: MSP430F2417 Hello everyone,
I am using a MSP430F2417 device and CCE. I was trying to build a code of fairly large size (approx 76k). I observed that the linker automatilcaaly splits the .text section into two sections:…