Part Number: MSP430F413 Tool/software: Code Composer Studio can i get example for 2 mux with 16 pin lcd
these 16 pins are connected to
P3SEL |= 0xF0;// Set the pin usage bits for the LCD P4SEL |= 0xFF; // Set the pin usage bits for the LCD P5SEL |= 0xA8;…
Part Number: MSP430F413
Saw the above statement on the MSP430x4xx Family Users Guide (slau056b).
Does it mean that the comparator input for MSP430F413 input Pin 47 (P16/CA0) need to connect a resistor
(100K) to ground when no signal is detected.
My current…
Part Number: MSP430F413 Tool/software: Code Composer Studio how to initialize the 2 mux lcd with 3 ports
LCDCTL = LCD2MUX + LCDSG0_1;
how to access the mory
LCDMEM[0]
Part Number: MSP430F413 Hi,
I am trying to understand this code which was written by a former staff who has left the company.
The code is as follows, somehow I got lost in the routine as to what it actually does :
; THIS IS A 16-BIT BY 16-BIT MULTIPLICATION…
Part Number: MSP430F413
hi,Msp430F413 work with 32KHZ, use the watchdog timer time work, program debugging found, each time the frequency is sometimes different, there are two cases, 10 times there are 2 times, the frequency is about 2/1. Don't know…
Part Number: MSP430F413
Hi TI employee,
My coustomer designed a watermeter with MSP430F413 . The problem is if the P1.2 IO interrupt occuers, it will affect P1.0, and make P1IFG = 0x03.
It 's easy reproduce this issue. Pls help check and give a solution…
Part Number: MSP430F413 Other Parts Discussed in Thread: MSP430F1111A
MSP430F413 : How does it work with analog signal directly into it?
I have to use MSP430F413 to display analog signal on a LCD display, but it hasn't any ADC, and I will not use a external…
Hello, pleasee anyone help me.
I'm having trouble making two interrupts work correctly in my code
the first refers to a clock, and the second to my UART communication
independent the two work properly, however when enabling the two at the same time…
Part Number: MSP430F4132 Tool/software: Code Composer Studio Has anyone had any experience here? For some reason I can't fathom, I can only get digits to display if all segments are turned on. For instance, loading 0x01, 0x02, 0x04 or 0x08 into LCDM1…
Part Number: MSP430F413 I have a test probe that reads the conductivity of a solution and have written a code
to read the conductivity and display on the LCD.
The probe needs to be calibrated to a 5 ppt level every time it is used.
I have encountered…