Part Number: TIDA-00120 Other Parts Discussed in Thread: MSP430F5152 , Tool/software: Code Composer Studio Hello,
I'm developing MPPT controller using MSP430F5152 based on TIDA-00120 reference design.
I modfied design from the original interleved Bu…
Part Number: MSP430F5152 Other Parts Discussed in Thread: MSP430WARE Tool/software: Code Composer Studio Hello MSP430 expert,
I've been designing MPPT controller by referring PMP7605 reference S/W using MSP430F5152 MCU.
As Timer D0/D1 is documented…
Part Number: MSP430F5152 Other Parts Discussed in Thread: CCSTUDIO Tool/software: Code Composer Studio Sir, I am working on MSP430f5152 mcu, i have writing a code in CCS v7. Now when i write a more code or increase the size of code the CCS not allow me…
Part Number: MSP430F5152 hi,
my customer's project using MSP430F5152 be the subsystem, they need extremally low power consumption,
their FW using the interrupt event to awake MSP430 from LPM, and most of time, the MSP430 is in LPM mode.
but they found…
Part Number: MSP430F5152 Dear all,
In my application, I want to use 5V Tolerant I/O by 3.3V and 5V I/O on MSP430F5152 as following.
- Leave the DVIO pin.
- Supply external pull-up source(3.3V or 5V) through a resistor on I/O line.
Is it possible?
Sincerely…
Part Number: MSP430F5152 hi,
as we know, in LPM, there's a difference of whether the DC Generator is turn off or not,
and if i'm right, keeping the dc generator on during LPM is the purpose for wakeup faster,
if so, how faster compare to when DC Gen…
Other Parts Discussed in Thread: MSP430F5152 CPU: MSP430F5152
MCLK: 25MHz
Power supply voltage: 5V
When code running at unlimited loop: while(1) { } The system power consumption is 2.8mA
When code running at unlimited loop:
while (1)
{
if(anything != 0…
Other Parts Discussed in Thread: MSP430F5152 hi
my design need to have one SPI master and one SPI slave on MSP430F5152, so i design USCI_A0 be the SPI master and USCI_B0 be the SPI slave.
and my SPI Slave need to be 4 wire type, but the UCB0STE and UCA0CLK…
Other Parts Discussed in Thread: MSP430F5152 HI,
i am using msp430f5152 for my project . i would like to read a series of analog inputs,for this purpose i used port P1.0 to 1.5 and also port 3.0 using portmapping functionality. But how do i include port…
Other Parts Discussed in Thread: MSP430F5152 , MSP430F5172 In the MSP430F5152 datasheet's BSL section it lists Data Transmit for the 40-pin QFN RSB package as P3.5 - 34 and P3.7 - 36. It eludes that a register setting would allow transmit to happen…