Part Number: MSP430F5171 Hy everybody, i'm asking here beacouse i think some developer could have some advice to give me.
I have done many applications using MSP430 family, all with success and reliability.
Generally i have to connect devices to PC…
Part Number: MSP430F5171 Tool/software: Code Composer Studio
Hello we need help please:
“When the code is compiled with Code Composer Studio Compiler version 5.5.0.00077 the code fits into the 32K device with 6.5kB of flash memory free.
When the…
Part Number: MSP430F5171 Hi Team,
I do mistake in the production (produce 60ku) and soldering 470pF instead of 470nF as recommended in the data sheet.
What can be cause? Maybe need to do heat & cold test in order to see if there is not extend in the current…
Part Number: MSP430F5171 Hi,
I have a problem with Unified Clock System module. When I wake-up MCU form low power state sometimes FLL loop can't catch correct frequency and DCOFFG flag in UCSCTL7 register is set. This is probably caused by incorrect DCO…
Part Number: MSP430F5171 My circuit works faithfully with its internal REFO of 32Khz, from wich i obtain a clock of 24.576Mhz.
I've seen that internal 32K reference has a precision of 1.5% and it is too much for a particular application.
Using a higher…
Hello Folks,
Please could let me know how long I need to hold the _RESET_ pin low for to trigger a reset on the MSP430-5171
I've looked through the data sheet but couldn't see anything.
Thanks,
Andy.
Other Parts Discussed in Thread: MSP430F5171 Hello everyone,
I am using an MSP430F5171, and I have UC B 0 configured as SPI Master running at 4 Mhz talking to an IMU.
I originally had UC A 0 configured as UART talking to a wireless module, but I determined…
Other Parts Discussed in Thread: MSP430F5171 , MSP-FET , ENERGYTRACE Hi, I have had the following problem a couple of times now. I have been trying to program my MSP430F5171 device using a TI programmer and the Elpotronic FET430pro (lite) software.
Typically…
Part Number: TMS320F280021 Other Parts Discussed in Thread: MSP430F5171 , Hy, i use CCS IDE for MSP430F5171
Now i'm planning to use TMS320F280021 and I'll buy its debugger XDS200 USB.
My CCS is set only for MSP430 familiy, how to make it able to…
Other Parts Discussed in Thread: MSP430F5171 , ASH 1321.Schematic.pdf I'm using a UM232R from FTDI to communicate to the MSP430F5171 bootloader and have the following connections:
MSP430 UM232R
RST# DTR# (# represents inverted signal)
TEST RTS#
Tx …