Other Parts Discussed in Thread: MSP430F5232 Hi guys!
I have read on MSP430F5232 Datasheet (revised Nov 2015) the next description of pin 21 on the page 14:
P2.7 / UCB0STE / UCA0CLK ; Pin 21 ; I/O; General-purpose digital IO , etc...
Well, on the rest…
Out of curiosity, were you able to get the F5232 working correctly with the EZFET lite software? I need just basic programming functionality with no back channel UART.
Thanks!
Other Parts Discussed in Thread: MSP-GANG , MSP-TS430RGZ48C , MSP430F5232 , MSP-FET , MSP-TS430RGC64C We have an MSP430F5232 on a board with JTAG connection, it will not program with either the new MSP-FET or with MSP-GANG Programmer. In addition, if I put…
Other Parts Discussed in Thread: MSP430F5232 Hi, I have several questions on the clock of MSP430F5232.
Is it necessary to place an external crystal to provide a clock? Or can I use only internal VLO to make uC work ?
The manual says that XT1 is up to 32kHz…
Other Parts Discussed in Thread: MSP430F5232 I have two questions on MSP430F5232's power design.
For MSP430F5232 , all three powers VCC/AVcc/DVcc are tied together with two capacitors of 10uF and 0.1uF according to the reference design in the user manual…
Other Parts Discussed in Thread: MSP430F5232 , MSP430F5529 , MSP430F5528 HI,
Do you have a reference design of MSP430F5232?
It will be useful to see how power and clock signals are routed as well as the data-lines.
Thank you.
Other Parts Discussed in Thread: MSP430F5232 , MSP430WARE Hi,
I am going to use MSP430F5232 for my design, and I need to purchase its evaluation board.
What I could find is MSP-FET430U64C. It seems to be a good candidate, but it is for 64-pin package.
…
Other Parts Discussed in Thread: MSP430F5232 , MSP430F5510 Hi.
On MSP430F5232, I am planning to use “4-pin JTAG mode”. I want to confirm which signals need to be used to enable this mode. Beside four JTAG signals (TDO, TDI, TMS, TCK), two control signals…
Other Parts Discussed in Thread: MSP430F5232 Hi,
I have several questions on the power and clock of MSP430F5232.
I could not find a reference design with MSP430F5232. Is there a reference design? I want to check how clocks and powers are provided in the…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: MSP430F5232 , , MSP430FR2311 Champs,
I am asking this for our customers.
We use FR2433 acting as SPI slave by eUSCI_A with UCCKPH=1,UCCKPL=0;
It's weird that sometimes the first bit of MISO is…