Other Parts Discussed in Thread: MSP430F5308 Hi,
We have a board with MSP430F5308 (64 leg version - MSP430F530xIRGC).
Under "Recommended Operating Conditions" in SLAS677E [SEPTEMBER 2010–REVISED NOVEMBER 2013] it is written that Capacitor…
Hi Johnson,
Yes - the TM4C123 ARM M4F runs a version of the Replicator code to program a MSP430F5526. It is NOT working.
On another board, the TM4C123 ARM M4F programs the MSP430F5308 and it is working.
The Replicator code dies in the EraseFLASH_430Xv2…
Hi, I'm trying to program this MSP430. I'm not 100% sure I have it wired correctly, but basically I have all Vcc and Vss connected to 3.3v and gnd respectively for power.
I'm using a launchpad instead of a MSP-FET430UIF until it comes in the mail…
Other Parts Discussed in Thread: TPS62730 , CC1120 Hello,
Our design is based on a coin cell battery.
Please advice what will be the recommended design for CC1120 & MSP430F5408 to be connected to TPS62730
In order to save as much power as possible?
Other Parts Discussed in Thread: MSP430F5308 Hi,
We are developing a product in which there are up to 10 MSP430F5308 boards connected as slaves on a single I2C bus. The I2C master is a STM32F207 ARM MCU. Every MSP slave board has an I2C repeater on it…
Other Parts Discussed in Thread: MSP430F5308 Below is some code for an MSP430F5308 that outputs ACLK on P1.0. When run though, the frequency of the output on P1.0 is 32.9 KHz
The signal at XIN (P5.4) has frequency of 32768 Hz. The signal on P1.1 has a frequency…
Other Parts Discussed in Thread: MSP430F5308 i do the firmware upgrade for msp430f5308 base on the slaa535a, i try using the lunchpad as the bridge which receive the PC script command and programming the target MSP430F5308, it works well.
But when i replace…
Other Parts Discussed in Thread: MSP430F5308 When i doing the FW upgrade in MSP430F5308 base on the way of slaa535, it works well when i use the launchpad as the bridge between PC side and the target MSP430F5308, and the normal feedback from MSP430 will…
Other Parts Discussed in Thread: MSP430F5308 , MSP430F5309 Hi everyone,
I am now doing a product on MSP430F530X.
The MCU I used to use is MSP430F5308.
For a new batch of the product, I change it to MSP430F5309 because MSP430F5308 is out of stock.
And from…
Other Parts Discussed in Thread: MSP430F5308 dear sir,
i Am trying to burn program in msp430f5308 by using ccs software. but when we connect it. it everytime shows an error i.e MSP430: Error connecting to the target: Unknown device and another problem…