Part Number: MSP430F5436 Hi experts,
Is there any way to reprogram MSP430/2 via JTAG through BSL after it is in the field with blown fuse? or do I have to replace a new MSP every time?
Thanks,
Connie
Other Parts Discussed in Thread: MSP430F5438 , MSP430F5436 Hello
i have MSP430F5436 EVM ,which have different schematics and software rather than MSP430F5438 EVM ,
i can't find any user guide ,schematics and software(User experience ) for MSP430F5436 on…
Hi,
We observe that the timing of units are drifting more than normal. Some of the units are slower while other units run faster than the correct time. The sample size is 5 units.
We make use of the MSP430's RTC_A module for time keeping. Also we have…
Other Parts Discussed in Thread: MSP430F5436 , MSP430F5436A Is the voltage to the RTC pins for the MSP430F5436 supplied through the VCC pins on the micro or is it supposed to be supplied externally.
Thanks
Other Parts Discussed in Thread: MAX232 Hi all,
We are using the titled device for a complex embedded low-power hand-held device, and have run into a recent issue where the reset I/O gets stuck hard low if left connected to the MSP-FET430UIF. The reset…
Other Parts Discussed in Thread: MSP430F5436 , MSP430F5436A , MSP430WARE Customer is not able to get the MSP430F5436 to work in LPM3 mode. Current they are measuring on the micro is about 90uA. Something prevents it from going into LPM3. They are using UCSCTL8…
Other Parts Discussed in Thread: MSP430F5436 I've been working for the past couple days on developing an ISP strategy for use with the MSP430F5436. I was testing and debugging this when suddenly I lost the ability to JTAG connect to the processor. …
Other Parts Discussed in Thread: MSP430F5436MSP430f5436 MICRO CODE SPACE
Can the msp430 compiler generate fully relocatable code for programs located above 64K in flash memory? We need a program linked to run in Bank 1 to be able to run in Bank 2 of…
Hi all, I'm new to this group. Be gentle :)
Has anyone experienced CCR4 of Timer B0 not being output on the port pin? I'm using 7 of Timer B's capture compare registers configured as PWO outputs on their respective port pins. CCR1 - CCR6 …
Hi,
I'm currently encountering an issue on the 5436 where code space from 0x30000 seems to be unreliable for 408 bytes.
In my application, data for initialisation is being stored there (and loaded into memory before main runs). I find that a fresh…