Other Parts Discussed in Thread: MSP430F5437 Hi,
I'm using an MSP430f5437 as modbus master and using a MAX3471 as RS485 transceiver.
and this is how I set the uart:
P3SEL = (BIT4+BIT5); // P3.4,5 = USCI_A0 TXD/RXD
UCA0CTL1…
Other Parts Discussed in Thread: MSP430F5437 , MSP430F5437A Hello TI,
I am trying to implement a 9600 baud rate UART on the MSP430F5437. I do see Table 34-4 in the following user guide that illustrates the settings: http://www.ti.com/lit/ug/slau208n/slau208n…
Hi friends,
I have ported the MSP430F5438A+CC2520 experimantal board zstack to LSR-ProFLEX01 zigbee module.
In experimental code, There are 6 GPIO from cc2520 connected to MSP430.
But In LSR-ProFLEX01 zigbee module, only 3 GPIO connected to msp430.
…
Other Parts Discussed in Thread: MSP430F5437 Hi all,
I am struggling with the VMAIFG and as I am NOT expecting it to be set, I guess it must be related to CPU20. The errata sheet seems to be updated on this matter 'recently' (last six months) with…
Other Parts Discussed in Thread: CC430F5137 , MSP430F5437 Hi all,
I've been looking for info at the forum but I can't really find a definitive answer.
I'm in the process of migrating an application from a CC430F5137 to an MSP430F4537 (it will be…
Other Parts Discussed in Thread: MSP430F5437 Hello,
I am new to TI MSP430F5437. I have some questions on MSP430F5437 chip.
I want to know how many external interrupt pins can it provides. Upon the data sheet and the user guide, port P1 and P2 can be…
Other Parts Discussed in Thread: MSP430F5437 I'm using a msp430f5437. Can I put this ucontroller to LMP3 if I'm using SMCLK soursed by DCO (default DCO 2Mhz) and ACLK soursed by REFOCLK? SMLK is used to source Timer A and ACLK source for Timer B.…
Other Parts Discussed in Thread: MSP430F5437 , CC1020 Dear all,
I'm new with MSP430F5437 and I'm not able to configure the SPI interface with the transceiver cc1020 (slave). These are the functions that a certain main calls:
//SPI interface initialization…
It seems that you are not getting any feedback from the processor ?
As always, there could be several reasons for no contact. I would use a check list like this:
- Is hardware correct (correct pins and levels) ?
- Try another RS232 driver - we have seen…
Other Parts Discussed in Thread: MSP430F5437 , CC2520 Hi,
I'm working with a module based on an MSP430F5437 and a CC2520. The radio is using SPI on USCI_B0, and I need to use the other 3 communications modules (F5437 has 4) for SPI as well.
Unfortunately…