Part Number: MSP430F5510
I need to know the requirements for selecting an external clock source (CMOS oscillator) for XT2 for USB. This design is considering a 4MHz clock source (this would also allow USB BSL due to auto-detect to set XT2 to bypass mode…
Part Number: MSP430F5510 Hi Team,
This problem occurs when I was downloading via USB BSL. Could you please tell me how to solve it?
Kind regards,
Katherine
Hello Johnson,
Sorry for my late reply, as I am out of office in CNY holiday.
This issue only occured in some devices, the fail rate is about 2%, there are more than 100pcs failed devices on our production line. We have analyzed those failed devices and…
Part Number: MSP430F5510 Other Parts Discussed in Thread: MSP430WARE Hi expert
Customer would like to use MSP430F5510 USB function. They plug the USB interface into computer and run 430 example project from msp430ware\usblib430\MSP430_USB_Software\MSP430_USB_API…
Part Number: MSP430F5510 Our customer is asking for Die Rev: T1 14k F
Kontron has three part numbers listed on its AVL:
MSP430F5510IRGC, MSP430F5510IRGCR, MSP430F5510IRGCT
How can we order per this request?
Part Number: MSP430F5510 Why do I get an error :"expected a declaration"
For there lines?
#define RB_INITIALIZE(rb) do { (rb).read_idx = 0; (rb).write_idx = 0; (rb).data_ct = 0; } while (0);
It seems to me a properly define routine.
erubin@tetracore…
Hello All,
The USB Descriptor tool is TI made and is used to help get supported HID types correctly on the PC you are using. We allow for a Custom category to expand to HID class types we don't natively support. Joystick/Gamepads fall into this category…
Part Number: MSP430F5510 We are using driverlib to program the UCS and Timer1_A3 to generate a PWM output. We are expecting a PWM period of 200uS, but when we check the PWM frequency with an oscilloscope we measure 100uS. This suggests that the timer…
Part Number: MSP430F5510 We are using MSP430F5xx_6xx driverlib Version 2.91.13.01 for MSP430F5510. We need to generate a BOR from S/W but we noticed that the PMM_trigBOR API does not exist on this device even though the associated PMM register bits exist…
Part Number: MSP430F5510 Other Parts Discussed in Thread: MSP-GANG Hi team,
The following problem occurs when saving the testcode from the following software interface to the image 1.0 with "Save to Image", and shows the shows the following error: ERROR352…