Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430F2618
Tool/software: Code Composer Studio
So, this is what the text looks like in my MSP430F6659 project. Note the text "__interrupt" is not highlighted as a reserved word.
…
Part Number: MSP430F6659 Other Parts Discussed in Thread: INA126 Hi
I get all FFF's and I tried all different setup commands, including the example in MSPware. An example code of what I tried is below. I am using a 128msec timer A to enable the A/D. If…
Hi Manoj,
any update on this issue? I assume that the issue has been solved as you didn't reply back on this thread anymore.
Please verify the given answer and let me know if this thread can be closed.
Thanks and best regards,
Britta
Part Number: MSP430F6659 Other Parts Discussed in Thread: CSD , MSP430WARE
Tool/software: Code Composer Studio
Hi, I'm having a hard time trying to alter one of the MSPware GRLIB driver to support the very common SSD1963. with a 480x272 color graphics…
The default font setting looks like it is coming from Eclipse. Interestingly it differs by hostOS. On my Mac it uses Monaco and there 1 and l are very different. On Windows it uses Consolas which is similar to what Notepad++ uses and there they look…
Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430F5529 , MSP430F5528 Hi Gents,
Is it possible to do communication between three MSP430F6659 on the same PCB via USB bus using a USB hub like TUSB2046?
If yes, is there an example what the minimum…
Part Number: MSP430F6659
I would like to clock(MCLK and SMCLK) my MSP430F6659 at 19.2 MHz and use the internally trimmed 32768 clock as the reference input to the DCO but when I try to set this it fails. I know about the oscillator fault flag problem…
Part Number: MSP430F6659
Here is the code involved, for the functions I'm calling, they're all found in DriverLib ( http://dev.ti.com/tirex/content/msp/MSP430Ware_3_60_00_10/driverlib/doc/MSP430F5xx_6xx/html/index.html ) (guide at http://dev.ti…
Part Number: MSP430F6659 Tool/software: Code Composer Studio I am using 16.384 Mhz crystal ... when i am operation at this clk MCU got hangup and show such error mentioned below.
No source available for "0x4"
No source available for "0x33ffe…
Part Number: MSP430F6659 Hello,
I want to use the USB BSL function to download new firmware to the device. My XT2 clock is 16Mhz. The app note says it auto detects 4,8,12 or 24Mhz. Somewhere, I once thought I saw 16Mhz was included, but I can't find that…