Part Number: MSP430F6659 Hello,
I want to use the USB BSL function to download new firmware to the device. My XT2 clock is 16Mhz. The app note says it auto detects 4,8,12 or 24Mhz. Somewhere, I once thought I saw 16Mhz was included, but I can't find that…
Part Number: MSP430F6659 Hi,
I am working with a unit that have th MSP430.
I got with the unit an INVOKE file to open before opening the SW of the MSP (to burn the code).
As I understand (and i do not understand much...) in order to burn the code to the…
Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430F5659 , MSP430F5658 , MSP430F6658 Hi,
I still struggling with getting the USB BSL to work. I changed the constant from 0F 05 0F 03 11 02 17 01 to 0F 05 0F 03 11 04 17 01 in the firmware for the…
Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430FR5969 Dear sir or madam,
Every now and then, I do an introduction in MSP430 in our company and the colleagues very often ask the transistor count of a MSP430.
Could you please answer this…
Part Number: MSP430F6659 Is there any way to indicate indirect addressing methods for the origin or destination of the DMA?
I will be wondering if Ican set a buffer which has the addresses that the DMA will use as the origin or destination. This kind of…
Part Number: MSP430F6659 Tool/software: TI C/C++ Compiler I get the following error in the console window.
Description Resource Path Location Type <a href=" processors.wiki.ti.com/.../10099"> program will not fit into available memory. placement…
Part Number: MSP430F6659 Hello Guys,
I have developing my one project using MSP430F6659.
In that i am using different different Interrupts in my project.
My question is how to set Interrupt Priority?
Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430F149 , MSP430WARE Hello All, I am communicate AT24C1024 EEPROM with MSP430F6659 Microcontroller. If i try to write 1 in LSB of my data then it may be microcontroller hang or it will rotate in…
Part Number: MSP430F6659 Other Parts Discussed in Thread: MSP430F149 , MSPBSL , Hello,
i want to use UART BSL in MSP 430f6659 device. I have done already it in msp430f149 device successfully using hardware shown in slau319.
1 . Can i use same BSL hardware…
Part Number: MSP430F6659 Hi,
I'm trying to work with a battery(super-cap) that will support the MSP controller, while the main power will shut down.
I wish the MSP to work in LPM when he's supplied from the battery.
Are there any roccomendations…