Part Number: MSP430F6733A Hi, all.
I intend to erase Information Memory B.
Describing in 7.2.1 of User's Guide SLAU208Q, "If LOCKA=1, segment A cannot be written or erased, and all information memory is protected from being segment erased".
Is…
Part Number: MSP430F6733A Hi Experts,
REFO spec is defined as below.
We want to use MSP430F67x at 3.3V while the spec is defined at 3.0V. Can we consider even at VCC = 3.3 V, fREFO max is +-1.5%?
And if they use the temperature range from -20…
Part Number: MSP430F6733A Hi,
lowest voltage and the uart can be clocked upto 460800 baud, with UCOS16 enabled, since it is exactly one sixteenth of the system clock. All other lower common baudrates are then also pure integer devisions without a fractional…
Part Number: MSP430F6779 Other Parts Discussed in Thread: MSP430F6733A , MSP-TS430PEU128
Hi experts,
My customer has created two custom sensor boards using MSP430F67719A and MSP430F6733A. Due to the board, there is a case where -VFS (about -1.2V or…
Hi, No, PMM will not work, please see the Table 5-12 in chapter 5.8.5. msp430f6736a.pdf The test conditions is | dDVCC/dt |<3 V/s, 3V/5ns drop too fast. But I can't give an exact answer what the performance of MCU when it drop below 1.8V at a rate of…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…