Hi all,
I am working on MSP430FE427 Energy meter using Demo2. The meter is almost completed and working perfectly. Finally, I activated the LEDs to blink as per the energy value. ( 3200 impulses/ 1kwhr ) . it is working filne for both debug and hex releases…
Other Parts Discussed in Thread: MSP430FE427 Hi
i am using msp430fe427. i tried to comm with PC by uart. i can not find suitable code or doc about msp430fe427 uart.
thanks for help...
Other Parts Discussed in Thread: MSP430FE427A How can I implement I2c communication in MSP430FE427A? Is there is any code examples? the chip only has UART and SPI
When I turn on voltage and current the resistor of divider resistive voltage burns, when not assemble resistor of voltage or current works normally. the problem is when I turn next. I follow the reference guide SLAA203C. Someone could help me ?
Other Parts Discussed in Thread: MSP430FE427 MCU: MSP430FE427 Current ACLK: 32Khz IDE: IAR
I want to change my current external clk or ACLK to a higher crystal like: 4 or 8 Mhz.
Based on the electrical characteristics (SLAS396C - Page 17), the maximum clk…
Other Parts Discussed in Thread: MSP430FE427 MCU: MSP430FE427
I have the below timer ISR, I would like to know what happens when TACCR0 rolls over?
What happens when TACCR0 = 65530 and when TIMER_INTERVAL = 35? Would TACCR0 be set to 30?
#pragma vector=…
Other Parts Discussed in Thread: MSP430FE427
Objective - I am trying to acquire the slowest timer count possible.
Environment
Board: MSP430FE427
IDE: IAR
Setup
ACLK is 32Khz
MCLK is 8 Mhz
Question
I know I can use the ACLK as an input to the Timer_A…
Other Parts Discussed in Thread: MSP430FE427 , CC2431 [Problem:
My problem relates to Serial port communication between MSP430FE427 & CC2431. I need to send some data (characters)through serial port in UART mode to CC2431 and then, it will again be sent…