Hello,
Have you tried reprogramming the device through an IDE like CCS or IAR with the firmware configured for the MSP430FE427A (ESP430CE1A) rather than just programming the device with the MSP430FE427 (ESP430CE1) firmware image? Which current channel…
Other Parts Discussed in Thread: MSP430FE427 Hello,
Is it possible to program any MSP430 Device with MSP430 Launch Pad as ICSP ?
I have MSP430FE427 with Spy-Bi Wire . Is there any this Official List available .? from IT
--Gurpreet
Other Parts Discussed in Thread: MSP430FE427 I have a question about the e-meter reference designs, specifically about the current inputs.
In fig 5 in SLAA517, i see that one of the I-input has the option to tie to ground with JP-5.
My question is: what…
Other Parts Discussed in Thread: MSP430FE427 , MSP430FE427A Hello
I am using the MSP430FE427 EVM and demo2 software and I am not reading the correct reactive energy which then leads to incorrect Irms, apparent energy and power factor numbers.
I have discovered…
Other Parts Discussed in Thread: MSP430FE427 I use chip is MSP430FE427 IAR version is IAR Embedded Workbench Kickstart for MSP430 5.20 When I compile SLAA203A DEMO2 program appeared Fatal Error [e89]: Too much object code produced (more than 0x1000 bytes)…
Other Parts Discussed in Thread: MSP430FE427 I use chip is MSP430FE427 IAR version is IAR Embedded Workbench Kickstart for MSP430 5.20 When I compile SLAA203A DEMO2 program appeared Fatal Error [e89]: Too much object code produced (more than 0x1000 bytes)…
Other Parts Discussed in Thread: MSP430FE427 Hi,
I am using the MSP430FE427 micro controller and MSP-FET430UIF for debuging, when i am tring to connect the targe it will be giving the following error.
Exception occurred during launch.
Reason: Failed…
Other Parts Discussed in Thread: MSP430FE427 Hello : I use the chip is MSP430FE427
I would like to ask whether SLAA203 burn into this program can be measured after MSP430 voltage current power I'm still testing but my LSD-FET430UIF_V2.1 (USB -based …
Other Parts Discussed in Thread: ISO721 , MSP430FE427 , ISO7242C , ISO7242M Hi everyone,
I'm using ISO721 (not ISO150) to design isolated FET interface (Ref: slaa184.pdf).
Please help me with another schematic!
Thank you so much!